C55XX CSL EXAMPLE
GPIO EXAMPLE DOCUMENTATION

GPIO EXAMPLE2 - INPUT PIN TEST

TEST DESCRIPTION:

This example code tests the GPIO(General Purpose Input Output) pin functionality as input pin. C5505/C5515 DSP is having 32 GPIO pins which can be configured as input or output. GPIO pin 11 is configured as input pin by this test code. For verifying the input functionality, a source is required which sends data to the GPIO pin configured as input pin. GPIO pin 4 is configured as output pin and is used as data source for pin 11. These two pins should be connected with a jumper on the EVM to facilitate the data loop back. Interrupts are enabled for the GPIO input pin to indicate the high signal on the input pin. A data value 1 is written to the GPIO pin4 which is loop backed to the pin11 and is read in the ISR. Test will be successful when the GPIO interrupt for pin11 is generated. Value read from the pin11 is also compared with the value written to the pin4 to announce the success of the test.

NOTE: PIN 1(GPIO_4) AND 2(GPIO_11) OF J22 ON VC5505 EVM SHOULD BE CONNECTED WITH JUMPER BEFORE RUNNING THIS TEST CODE.

NOTE: PIN 1(GPIO_4) AND 2(GPIO_11) OF J13 ON C5515 EVM SHOULD BE CONNECTED WITH JUMPER BEFORE RUNNING THIS TEST CODE.

NOTE: THIS TEST HAS BEEN DEVELOPED TO WORK WITH CHIP VERSIONS C5505 AND C5515. MAKE SURE THAT PROPER CHIP VERSION MACRO IS DEFINED IN THE FILE c55xx_csl\inc\csl_general.h.

TEST PROCEDURE:

TEST RESULT: