Resistance temperature compensation optimizer, rev=3.44		
		
Optimized Impedance Track parameters:		
		
Qmax, mAh : 8079		
		
Ra table normalized to 25C, uncompressed, unscaled		
		
DOD, %	Ra, mOhm	
		
0	169	
11.11	169	
22.22	169	
33.33	171	
44.44	183	
55.56	177	
66.67	183	
77.78	191	
80.95	194	
84.13	201	
87.3	215	
90.48	234	
93.65	373	
96.83	663	
100	921	
		
Ra0_ch, mOhm : -31	This firmware is not explicitly supporting Ra0_ch, FCC drop could occur at low temperatures if used	
		
Thermal parameters:		
		
Temp a	1	
Temp k	-16.67	
		
Optimized resistance temperature compensation parameters saved in chemdat12		
		
		
Due to GG file format issues, GG values have not been updated		
		
		
Warning: Automatic firmware properties detection failed. Rb_select defaults to 2. Please make sure that chem ID loaded in the GG file is the same as ID specified in the config.txt		
Warning: Automatic firmware properties detection failed. basescale defaults to 1. Please make sure that chem ID loaded in the GG file is the same as ID specified in the config.txt