|
|
|
This example is intended to be a starting point for new development where a fuller set of kernel features and debug capabilities are enabled.
Board_LED0 - Indicates that the board was initialized within main()Board_LED0 as part of the initialization in main(). Then a heartBeat task toggles the LED at a rate determined by the arg0 parameter for the constructed Task instance in the .c file.This examples is the same as the Empty_Minimal example except many development and debug features are enabled. For example:
The ROM is being used in this example. This is controlled by the following lines in the .cfg file:
var ROM = xdc.useModule('ti.sysbios.rom.ROM'); if (Program.cpu.deviceName.match(/CC26/)) { ROM.romName = ROM.CC2650; } else if (Program.cpu.deviceName.match(/CC13/)) { ROM.romName = ROM.CC1350; }
Since the kernel in the ROM is being used, there is no logging or assert checking done by the kernel.
For IAR users using any SensorTag(STK) Board, the XDS110 debugger must be selected with the 4-wire JTAG connection within your projects’ debugger configuration.
For GNU and IAR users, please read the following website for details about enabling semi-hosting in order to view console output.
Please refer to the Memory Footprint Reduction section in the TI-RTOS User Guide spruhd4.pdf for a complete and detailed list of the differences between the empty minimal and empty projects.