|
Capacitive Touch Library
Description of the Capacitive Touch Library
|
Modules | |
| CTS_support | |
Functions | |
| void | TI_CAPT_Raw (const struct Sensor *groupOfElements, uint16_t *counts) |
| Measure the capacitance of each element within the Sensor. | |
| void | TI_CAPT_Init_Baseline (const struct Sensor *groupOfElements) |
| Make a single capacitance meausrment to initialize baseline tracking. | |
| void | TI_CAPT_Update_Baseline (const struct Sensor *groupOfElements, uint8_t numberOfAverages) |
| Update baseline tracking by averaging several measurements. | |
| void | TI_CAPT_Reset_Tracking (void) |
| Reset the Baseline Tracking algorithm to the default state. | |
| void | TI_CAPT_Update_Tracking_DOI (uint8_t direction) |
| Update the Baseline Tracking algorithm Direction of Interest. | |
| void | TI_CAPT_Update_Tracking_Rate (uint8_t rate) |
| Update the baseling tracking algorithm tracking rates. | |
| void | TI_CAPT_Custom (const struct Sensor *groupOfElements, uint16_t *deltaCnt) |
| Measure the change in capacitance of the Sensor. | |
| uint8_t | TI_CAPT_Button (const struct Sensor *groupOfElements) |
| Determine if a button is being pressed. | |
| struct Element * | TI_CAPT_Buttons (const struct Sensor *groupOfElements) |
| Determine which button if any is being pressed. | |
| uint16_t | TI_CAPT_Slider (const struct Sensor *groupOfElements) |
| Determine the position on a slider. | |
| uint16_t | TI_CAPT_Wheel (const struct Sensor *groupOfElements) |
| Determine the position on a wheel. | |
| uint8_t TI_CAPT_Button | ( | const struct Sensor * | groupOfElements | ) |
Determine if a button is being pressed.
| groupOfElements | Pointer to button to be scanned |
| struct Element* TI_CAPT_Buttons | ( | const struct Sensor * | groupOfElements | ) | [read] |
Determine which button if any is being pressed.
| groupOfElements | Pointer to buttons to be scanned |
| void TI_CAPT_Custom | ( | const struct Sensor * | groupOfElements, |
| uint16_t * | deltaCnt | ||
| ) |
Measure the change in capacitance of the Sensor.
This function measures the change in capacitance of each element within a sensor and updates the baseline tracking in the event that no change exceeds the detection threshold. The order of the elements within the Sensor structure is arbitrary but must be consistent between the application and configuration. The first element in the array (deltaCnt) corresponds to the first element within the Sensor structure.
| groupOfElements | Pointer to Sensor structure to be measured |
| deltaCnt | Address to where the measurements are to be written |
| void TI_CAPT_Init_Baseline | ( | const struct Sensor * | groupOfElements | ) |
Make a single capacitance meausrment to initialize baseline tracking.
| groupOfElements | Pointer to Sensor structure to be measured |
| void TI_CAPT_Raw | ( | const struct Sensor * | groupOfElements, |
| uint16_t * | counts | ||
| ) |
Measure the capacitance of each element within the Sensor.
This function selects the appropriate HAL to perform the capacitance measurement based upon the halDefinition found in the sensor structure. The order of the elements within the Sensor structure is arbitrary but must be consistent between the application and configuration. The first element in the array (counts) corresponds to the first element within the Sensor structure.
| groupOfElements | Pointer to Sensor structure to be measured |
| counts | Address to where the measurements are to be written |
| void TI_CAPT_Reset_Tracking | ( | void | ) |
Reset the Baseline Tracking algorithm to the default state.
| none |
| uint16_t TI_CAPT_Slider | ( | const struct Sensor * | groupOfElements | ) |
Determine the position on a slider.
| groupOfElements | Pointer to slider |
| void TI_CAPT_Update_Baseline | ( | const struct Sensor * | groupOfElements, |
| uint8_t | numberOfAverages | ||
| ) |
Update baseline tracking by averaging several measurements.
| groupOfElements | Pointer to Sensor structure to be measured |
| numberofAverages | Number of measurements to be averaged |
| void TI_CAPT_Update_Tracking_DOI | ( | uint8_t | direction | ) |
Update the Baseline Tracking algorithm Direction of Interest.
| direction | Direction of increasing or decreasing capacitance |
| void TI_CAPT_Update_Tracking_Rate | ( | uint8_t | rate | ) |
Update the baseling tracking algorithm tracking rates.
| rate | Rate of tracking changes in and against direction of intrest |
| uint16_t TI_CAPT_Wheel | ( | const struct Sensor * | groupOfElements | ) |
Determine the position on a wheel.
| groupOfElements | Pointer to wheel |
1.7.3