//***************************************************************************** // // Linker configuration file for CC2538. // // Copyright (c) 2012-2013 Texas Instruments Incorporated. All rights reserved. // //***************************************************************************** // // Define a memory region that covers the entire 4 GB addressible space of the // processor. // define memory mem with size = 4G; // // Define a region for the on-chip program code space. // define region FLASH = mem:[from 0x00200000 to 0x0023C7FF]; // // Define a region for the OTA CRC structure. // //define region CRC = mem:[from 0x002001EC to 0x002001F3]; // // Define a region for the OTA Preamble structure. // //define region PREAMBLE = mem:[from 0x002001F4 to 0x002001FF]; // // Define a region for the NVIC table that is 512-byte aligned. // //define region INTVEC = mem:[from 0x00200200 to 0x002003FF]; // // Define a region for the on-chip non-volatile (NV) memory. // "HAL_NV_PAGE_CNT" pages of on-chip flash memory (originally 6 pages) are // designated for Z-Stack NV items to be stored outside program code space. // The size of this region MUST MATCH the size defined by "HAL_NV_PAGE_CNT" // in the file: hal_board_cfg.h // define region NV_MEM = mem:[from 0x0023C800 to 0x0023F7FF]; // // Define regions for on-chip factory Commissioning Parameters. // One page of on-chip flash memory (originally page 255) is designated // for various parameters to be "commissioned" outside program code space. // // Key-Establishment "Implicit Certificate 283" define region CP_IMPC_283 = mem:[from 0x0023FED4 to 0x0023FF1F]; // // Key-Establishment "Certificate Authority Public Key 283" define region CP_CAPK_283 = mem:[from 0x0023FF20 to 0x0023FF47]; // // Key-Establishment "Device Private Key 283" define region CP_DEPK_283 = mem:[from 0x0023FF48 to 0x0023FF6B]; // // Key-Establishment "Implicit Certificate" define region CP_IMPC = mem:[from 0x0023FF6C to 0x0023FF9B]; // // Key-Establishment "Certificate Authority Public Key" define region CP_CAPK = mem:[from 0x0023FF9C to 0x0023FFB3]; // // Key-Establishment "Device Private Key" define region CP_DEPK = mem:[from 0x0023FFB4 to 0x0023FFCB]; // // Device's unique 64-bit IEEE address define region CP_IEEE = mem:[from 0x0023FFCC to 0x0023FFD3]; // // Define a region for Customer Configuration Area in flash. define region FLASH_CCA = mem:[from 0x0023FFD4 to 0x0023FFDF]; // // Define the region for Lock Bits in flash. define region FLASH_LCK = mem:[from 0x0023FFE0 to 0x0023FFFF]; // // Define the region for Image Boot Manager (IBM) Ledger Page. //define region LEDGER_PAGE = mem:[from 0x0023C000 to 0x0023C7FF]; // // Define the region for Image Boot Manager (IBM) //define region BOOTLOADER_PAGE = mem:[from 0x0023F800 to 0x0023FD00]; // // Define a region for the on-chip SRAM. // define region SRAM = mem:[from 0x20004000 to 0x20007FFF]; // // Define a block for the heap. The size should be set to something other // than zero if things in the C library that require the heap are used. // define block HEAP with alignment = 8, size = 0x00000100 { }; // // Indicate that the read/write values should be initialized by copying from // flash. // initialize by copy { readwrite }; // // Indicate that the noinit values should be left alone. This includes the // stack, which if initialized will destroy the return address from the // initialization code, causing the processor to branch to zero and fault. // do not initialize { section .noinit }; // // Place the OTA CRC structure. // //place at start of CRC { readonly section .crc }; // // Place the OTA Preamble structure. // //place at start of PREAMBLE { readonly section .preamble }; // // Place the interrupt vectors. // place at start of FLASH { readonly section .intvec }; // // Place the cca area at the end of flash. // place at start of FLASH_CCA { readonly section .cca }; // // Place the commissioning parameter items. // place at start of CP_IEEE { readonly section IEEE_ADDRESS_SPACE }; place at start of CP_DEPK { readonly section DEV_PRIVATE_KEY_ADDRESS_SPACE }; place at start of CP_CAPK { readonly section CA_PUBLIC_KEY_ADDRESS_SPACE }; place at start of CP_IMPC { readonly section IMPLICIT_CERTIFICATE_ADDRESS_SPACE }; place at start of CP_DEPK_283 { readonly section PRIV_KEY_283_ADDRESS_SPACE }; place at start of CP_CAPK_283 { readonly section CA_PUB_KEY_283_ADDRESS_SPACE }; place at start of CP_IMPC_283 { readonly section IMPL_CERT_283_ADDRESS_SPACE }; // // Place the remainder of the read-only items into flash. // place in FLASH { readonly }; // // Place the RAM vector table at the start of SRAM. // place at start of SRAM { section VTABLE }; // // Place all read/write items into SRAM. // place in SRAM { readwrite, block HEAP }; // // Place the ledger page, if it's defined // //place at start of LEDGER_PAGE { section .ledger }; //do not initialize { section .ledger }; // // Place the bootloader page, if it's defined startup_ewarm // //place at start of BOOTLOADER_PAGE { section .bootloader };