Int32 Setup_Rx (Void) { Int32 result, vectId; UInt8 isAllocated, accChannelNum, i; UInt16 numAccEntries, intThreshold; Qmss_Queue rxFreeQInfo, rxQInfo; Ptr pCppiDesc; Qmss_AccCmdCfg accCfg; Cppi_RxFlowCfg rxFlowCfg; Int16 eventId; Ptr pDataBuffer; Uint32 mySWInfo[] = {0x11112222, 0x33334444}; /* Open a Receive (Rx) queue. * * This queue will be used to hold all the packets received by PASS/CPSW * * Open the next available High Priority Accumulation queue for Rx. */ if ((gRxQHnd = Qmss_queueOpen (Qmss_QueueType_HIGH_PRIORITY_QUEUE, QMSS_PARAM_NOT_SPECIFIED, &isAllocated)) < 0) { System_printf ("Error opening a High Priority Accumulation Rx queue \n"); return -1; } rxQInfo = Qmss_getQueueNumber (gRxQHnd); /* Setup high priority accumulation interrupts on the Rx queue. * * Let's configure the accumulator with the following settings: * (1) Interrupt pacing disabled. * (2) Interrupt on every received packet */ intThreshold = RX_INT_THRESHOLD; numAccEntries = (intThreshold + 1) * 2; accChannelNum = PA_ACC_CHANNEL_NUM; /* Initialize the accumulator list memory */ memset ((Void *) gHiPriAccumList, 0, numAccEntries * 4); /* Ensure that the accumulator channel we are programming is not * in use currently. */ result = Qmss_disableAccumulator (Qmss_PdspId_PDSP1, accChannelNum); if (result != QMSS_ACC_SOK && result != QMSS_ACC_CHANNEL_NOT_ACTIVE) { System_printf ("Error Disabling high priority accumulator for channel : %d error code: %d\n", accChannelNum, result); return -1; } /* Setup the accumulator settings */ accCfg.channel = accChannelNum; accCfg.command = Qmss_AccCmd_ENABLE_CHANNEL; accCfg.queueEnMask = 0; accCfg.listAddress = Convert_CoreLocal2GlobalAddr((Uint32) gHiPriAccumList); accCfg.queMgrIndex = gRxQHnd; accCfg.maxPageEntries = (intThreshold + 1); /* Add an extra entry for holding the entry count */ accCfg.timerLoadCount = 0; accCfg.interruptPacingMode = Qmss_AccPacingMode_LAST_INTERRUPT; accCfg.listEntrySize = Qmss_AccEntrySize_REG_D; accCfg.listCountMode = Qmss_AccCountMode_ENTRY_COUNT; accCfg.multiQueueMode = Qmss_AccQueueMode_SINGLE_QUEUE; /* Program the accumulator */ if ((result = Qmss_programAccumulator (Qmss_PdspId_PDSP1, &accCfg)) != QMSS_ACC_SOK) { System_printf ("Error Programming high priority accumulator for channel : %d queue : %d error code : %d\n", accCfg.channel, accCfg.queMgrIndex, result); return -1; } /* Register interrupts for the system event corresponding to the * accumulator channel we are using. */ /* System event 48 - Accumulator Channel 0 */ eventId = 48; /* Pick a interrupt vector id to use */ vectId = 7; /* Register our ISR handle for this event */ EventCombiner_dispatchPlug (eventId, (EventCombiner_FuncPtr)Cpsw_RxISR, (UArg)NULL, TRUE); /* Map the combiner's output event id (evevtId/32) to hardware interrupt 8. */ /* The HW int 8 is slected via CM.eventGroupHwiNum[] specified at cpsw_example.cfg */ Hwi_eventMap(vectId, 1); /* Enable interrupt 8. */ Hwi_enableInterrupt(vectId); /* Open a Rx Free Descriptor Queue (Rx FDQ). * * This queue will hold all the Rx free decriptors. These descriptors will be * used by the PASS CPDMA to hold data received via CPSW. */ if ((gRxFreeQHnd = Qmss_queueOpen (Qmss_QueueType_STARVATION_COUNTER_QUEUE, QMSS_PARAM_NOT_SPECIFIED, &isAllocated)) < 0) { System_printf ("Error opening Rx Free descriptor queue \n"); return -1; } rxFreeQInfo = Qmss_getQueueNumber (gRxFreeQHnd); /* Attach some free descriptors to the Rx free queue we just opened. */ for (i = 0; i < NUM_RX_DESC; i++) { /* Get a free descriptor from the global free queue we setup * during initialization. */ if ((pCppiDesc = Qmss_queuePop (gGlobalFreeQHnd)) == NULL) { break; } /* The descriptor address returned from the hardware has the * descriptor size appended to the address in the last 4 bits. * * To get the true descriptor size, always mask off the last * 4 bits of the address. */ pCppiDesc = (Ptr) ((UInt32) pCppiDesc & 0xFFFFFFF0); if ((pDataBuffer = (Ptr) Memory_alloc(NULL, 1518, 0, NULL)) == NULL) { System_printf ("Error allocating memory for Rx data buffer \n"); break; } /* Populate the Rx free descriptor with the buffer we just allocated. */ Cppi_setData (Cppi_DescType_HOST, pCppiDesc, (UInt8 *)Convert_CoreLocal2GlobalAddr((UInt32)pDataBuffer), 1518); /* Save original buffer information */ Cppi_setOriginalBufInfo (Cppi_DescType_HOST, pCppiDesc, (UInt8 *)Convert_CoreLocal2GlobalAddr((UInt32)pDataBuffer), 1518); /* Setup the Completion queue: * * Setup the return policy for this desc to return to the free q we just * setup instead of the global free queue. */ Cppi_setReturnQueue (Cppi_DescType_HOST, pCppiDesc, rxFreeQInfo); Cppi_setSoftwareInfo (Cppi_DescType_HOST, pCppiDesc, (UInt8 *) mySWInfo); Cppi_setPacketLen (Cppi_DescType_HOST, pCppiDesc, 1518); /* Push descriptor to Tx free queue */ Qmss_queuePushDescSize (gRxFreeQHnd, pCppiDesc, SIZE_HOST_DESC); } if (i != NUM_RX_DESC) { System_printf ("Error allocating Rx free descriptors \n"); return -1; } /* Setup a Rx Flow. * * A Rx flow encapsulates all relevant data properties that CPDMA would * have to know in order to succefully receive data. */ /* Initialize the flow configuration */ memset (&rxFlowCfg, 0, sizeof(Cppi_RxFlowCfg)); /* Let CPPI pick the next available flow */ rxFlowCfg.flowIdNum = CPPI_PARAM_NOT_SPECIFIED; rxFlowCfg.rx_dest_qmgr = rxQInfo.qMgr; rxFlowCfg.rx_dest_qnum = rxQInfo.qNum; rxFlowCfg.rx_desc_type = Cppi_DescType_HOST; rxFlowCfg.rx_ps_location = Cppi_PSLoc_PS_IN_DESC; rxFlowCfg.rx_psinfo_present = 1; /* Enable PS info */ rxFlowCfg.rx_error_handling = 0; /* Drop the packet, do not retry on starvation by default */ rxFlowCfg.rx_einfo_present = 1; /* EPIB info present */ rxFlowCfg.rx_dest_tag_lo_sel = 0; /* Disable tagging */ rxFlowCfg.rx_dest_tag_hi_sel = 0; rxFlowCfg.rx_src_tag_lo_sel = 0; rxFlowCfg.rx_src_tag_hi_sel = 0; rxFlowCfg.rx_size_thresh0_en = 0; /* By default, we disable Rx Thresholds */ rxFlowCfg.rx_size_thresh1_en = 0; /* By default, we disable Rx Thresholds */ rxFlowCfg.rx_size_thresh2_en = 0; /* By default, we disable Rx Thresholds */ rxFlowCfg.rx_size_thresh0 = 0x0; rxFlowCfg.rx_size_thresh1 = 0x0; rxFlowCfg.rx_size_thresh2 = 0x0; rxFlowCfg.rx_fdq0_sz0_qmgr = rxFreeQInfo.qMgr; /* Setup the Receive free queue for the flow */ rxFlowCfg.rx_fdq0_sz0_qnum = rxFreeQInfo.qNum; rxFlowCfg.rx_fdq0_sz1_qnum = 0x0; rxFlowCfg.rx_fdq0_sz1_qmgr = 0x0; rxFlowCfg.rx_fdq0_sz2_qnum = 0x0; rxFlowCfg.rx_fdq0_sz2_qmgr = 0x0; rxFlowCfg.rx_fdq0_sz3_qnum = 0x0; rxFlowCfg.rx_fdq0_sz3_qmgr = 0x0; rxFlowCfg.rx_fdq1_qnum = rxFreeQInfo.qNum; /* Use the Rx Queue to pick descriptors */ rxFlowCfg.rx_fdq1_qmgr = rxFreeQInfo.qMgr; rxFlowCfg.rx_fdq2_qnum = rxFreeQInfo.qNum; /* Use the Rx Queue to pick descriptors */ rxFlowCfg.rx_fdq2_qmgr = rxFreeQInfo.qMgr; rxFlowCfg.rx_fdq3_qnum = rxFreeQInfo.qNum; /* Use the Rx Queue to pick descriptors */ rxFlowCfg.rx_fdq3_qmgr = rxFreeQInfo.qMgr; /* Configure the Rx flow */ if ((gRxFlowHnd = Cppi_configureRxFlow (gCpdmaHnd, &rxFlowCfg, &isAllocated)) == NULL) { System_printf ("Error configuring Rx flow \n"); return -1; } /* All done with Rx configuration. Return success. */ return 0; }