U-Boot SPL 2013.01.01 (Dec 15 2014 - 14:01:16) ### Use AM335x_SK V1.2 setting ### am335x_skmusb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb_init_controller failed with status -22 musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB OTG mode controller at 47401800 using PIO, IRQ 0 OMAP SD/MMC: 0 U-Boot SPL 2013.01.01 (Dec 15 2014 - 14:01:16) ### Use AM335x_SK V1.2 setting ### am335x_skmusb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Peripheral mode controller at 47401000 using PIO, IRQ 0 musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Host mode controller at 47401800 using PIO, IRQ 0 OMAP SD/MMC: 0 reading u-boot.img reading u-boot.img U-Boot 2013.01.01 (Dec 15 2014 - 14:01:16) I2C: ready DRAM: 256 MiB WARNING: Caches not enabled ### Use AM335x_SK V1.2 setting ### NAND: No NAND device found!!! 0 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 *** Warning - readenv() failed, using default environment musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Peripheral mode controller at 47401000 using PIO, IRQ 0 musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Host mode controller at 47401800 using PIO, IRQ 0 Net: not set. Validating first E-fuse MAC PHY reset timed out cpsw, usb_ether Hit any key to stop autoboot: 0 mmc0 is current device SD/MMC found on device 0 reading uEnv.txt 153 bytes read in 4 ms (37.1 KiB/s) Loaded environment from uEnv.txt Importing environment from mmc ... Running uenvcmd ... reading uImage 3526616 bytes read in 386 ms (8.7 MiB/s) ## Booting kernel from Legacy Image at 82000000 ... Image Name: Linux-3.2.0 Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 3526552 Bytes = 3.4 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK Loading Kernel Image ... OK OK Starting kernel ... Uncompressing Linux... done, booting the kernel. [ 0.000000] Linux version 3.2.0 (root@alan-virtual-machine) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #2 Fri May 20 09:22:03 CST 2016 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine: am335xevm [ 0.000000] Memory policy: ECC disabled, Data cache writeback [ 0.000000] AM335X ES2.1 (neon ) [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 mem=256M rootwait [ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes) [ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) [ 0.000000] Memory: 256MB = 256MB total [ 0.000000] Memory: 252612k/252612k available, 9532k reserved, 0K highmem [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB) [ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB) [ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB) [ 0.000000] .text : 0xc0008000 - 0xc0633000 (6316 kB) [ 0.000000] .init : 0xc0633000 - 0xc0672000 ( 252 kB) [ 0.000000] .data : 0xc0672000 - 0xc06e1e10 ( 448 kB) [ 0.000000] .bss : 0xc06e1e34 - 0xc0712cbc ( 196 kB) [ 0.000000] NR_IRQS:396 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz [ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz [ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms [ 0.000000] Console: colour dummy device 80x30 [ 0.000122] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144) [ 0.058959] pid_max: default: 32768 minimum: 301 [ 0.059082] Security Framework initialized [ 0.059173] Mount-cache hash table entries: 512 [ 0.059539] CPU: Testing write buffer coherency: ok [ 0.080047] omap_hwmod: gfx: failed to hardreset [ 0.096343] omap_hwmod: pruss: failed to hardreset [ 0.097442] print_constraints: dummy: [ 0.097808] NET: Registered protocol family 16 [ 0.099945] OMAP GPIO hardware version 0.1 [ 0.102508] omap_mux_init: Add partition: #1: core, flags: 0 [ 0.104431] omap_i2c.1: alias fck already exists [ 0.105285] omap2_mcspi.1: alias fck already exists [ 0.105529] omap2_mcspi.2: alias fck already exists [ 0.106445] edma.0: alias fck already exists [ 0.106475] edma.0: alias fck already exists [ 0.106475] edma.0: alias fck already exists [ 0.137634] bio: create slab at 0 [ 0.139892] SCSI subsystem initialized [ 0.141479] usbcore: registered new interface driver usbfs [ 0.141815] usbcore: registered new interface driver hub [ 0.141998] usbcore: registered new device driver usb [ 0.142150] musb-ti81xx musb-ti81xx: musb0, board_mode=0x11, plat_mode=0x1 [ 0.142425] musb-ti81xx musb-ti81xx: musb1, board_mode=0x11, plat_mode=0x1 [ 0.143585] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz [ 0.145446] tps65910 1-002d: JTAGREVNUM 0x0 [ 0.147857] print_constraints: VRTC: [ 0.149291] print_constraints: VIO: at 1500 mV [ 0.151611] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal [ 0.153900] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal [ 0.154907] print_constraints: VDD3: 5000 mV [ 0.156311] print_constraints: VDIG1: at 1800 mV [ 0.157745] print_constraints: VDIG2: at 1800 mV [ 0.159179] print_constraints: VPLL: at 1800 mV [ 0.160583] print_constraints: VDAC: at 1800 mV [ 0.162017] print_constraints: VAUX1: at 1800 mV [ 0.163452] print_constraints: VAUX2: at 3300 mV [ 0.164886] print_constraints: VAUX33: at 3300 mV [ 0.166320] print_constraints: VMMC: at 3300 mV [ 0.166809] tps65910 1-002d: No interrupt support, no core IRQ [ 0.168151] Advanced Linux Sound Architecture Driver Version 1.0.24. [ 0.168945] Sangoma WANPIPE Router v1.1 (c) 1995-2000 Sangoma Technologies Inc. [ 0.169403] Switching to clocksource gp timer [ 0.185058] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host) [ 0.185180] musb-hdrc musb-hdrc.0: dma type: pio [ 0.185485] MUSB0 controller's USBSS revision = 4ea20800 [ 0.185516] musb0: Enabled SW babble control [ 0.185699] musb-hdrc musb-hdrc.0: MUSB HDRC host driver [ 0.185791] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1 [ 0.185913] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 0.185943] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 0.185943] usb usb1: Product: MUSB HDRC host driver [ 0.185974] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd [ 0.185974] usb usb1: SerialNumber: musb-hdrc.0 [ 0.186767] hub 1-0:1.0: USB hub found [ 0.186798] hub 1-0:1.0: 1 port detected [ 0.187347] musb-hdrc musb-hdrc.0: USB Host mode controller at d083c000 using PIO, IRQ 18 [ 0.187530] musb-hdrc musb-hdrc.1: dma type: pio [ 0.187835] MUSB1 controller's USBSS revision = 4ea20800 [ 0.187835] musb1: Enabled SW babble control [ 0.188018] musb-hdrc musb-hdrc.1: MUSB HDRC host driver [ 0.188049] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2 [ 0.188140] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002 [ 0.188140] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 0.188171] usb usb2: Product: MUSB HDRC host driver [ 0.188171] usb usb2: Manufacturer: Linux 3.2.0 musb-hcd [ 0.188171] usb usb2: SerialNumber: musb-hdrc.1 [ 0.188934] hub 2-0:1.0: USB hub found [ 0.188964] hub 2-0:1.0: 1 port detected [ 0.189544] musb-hdrc musb-hdrc.1: USB Host mode controller at d083e800 using PIO, IRQ 19 [ 0.189971] NET: Registered protocol family 2 [ 0.190185] IP route cache hash table entries: 2048 (order: 1, 8192 bytes) [ 0.190490] TCP established hash table entries: 8192 (order: 4, 65536 bytes) [ 0.190643] TCP bind hash table entries: 8192 (order: 3, 32768 bytes) [ 0.190734] TCP: Hash tables configured (established 8192 bind 8192) [ 0.190765] TCP reno registered [ 0.190765] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.190795] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.190979] NET: Registered protocol family 1 [ 0.191253] RPC: Registered named UNIX socket transport module. [ 0.191253] RPC: Registered udp transport module. [ 0.191253] RPC: Registered tcp transport module. [ 0.191284] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.191497] NetWinder Floating Point Emulator V0.97 (double precision) [ 0.202667] VFS: Disk quotas dquot_6.5.2 [ 0.202758] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.203521] msgmni has been set to 493 [ 0.206634] alg: No test for stdrng (krng) [ 0.207305] io scheduler noop registered [ 0.207305] io scheduler deadline registered [ 0.207397] io scheduler cfq registered (default) [ 0.208587] Could not set LED4 to fully on [ 0.210357] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0 [ 0.907104] console [ttyO0] enabled [ 0.911376] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1 [ 0.919189] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2 [ 0.926971] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3 [ 0.934783] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4 [ 0.942565] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5 [ 0.950836] omap4_rng omap4_rng: OMAP4 Random Number Generator ver. 2.00 [ 0.967163] brd: module loaded [ 0.975158] loop: module loaded [ 0.978637] i2c-core: driver [tsl2550] using legacy suspend method [ 0.985107] i2c-core: driver [tsl2550] using legacy resume method [ 0.991546] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 1.050201] No daughter card found [ 1.053802] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 1.061065] Board name: A335X_SK [ 1.064422] Board version: 1.2B [ 1.067718] The board is a AM335x Starter Kit. [ 1.073028] alanaalalana EVM_SK [ 1.076263] omap_hsmmc.0: alias fck already exists [ 1.081909] omap_hsmmc.1: alias fck already exists [ 1.088531] davinci-mcasp.1: alias fck already exists [ 1.094299] 4G POWER OFF!!!!!!!!!!! [ 3.094726] 4G POWER ON!!!!!!!!!!! [ 3.597473] LEDCTL POWERON!!!!!!!!!!! [ 3.603942] _regulator_get: 1-0018 supply Vdd not found, using dummy regulator [ 3.611541] _regulator_get: 1-0018 supply Vdd_IO not found, using dummy regulator [ 3.639587] lis3lv02d: unknown sensor type 0x87 [ 3.644409] lis3lv02d_i2c: probe of 1-0018 failed with error -22 [ 3.653137] mtdoops: mtd device (mtddev=name/number) must be supplied [ 3.660308] omap2-nand driver initializing [ 3.664764] OneNAND driver initializing [ 3.670013] CAN device driver interface [ 3.674072] CAN bus driver for Bosch D_CAN controller 1.0 [ 3.730102] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 [ 3.736541] davinci_mdio davinci_mdio.0: no live phy, scanning all [ 3.743316] davinci_mdio: probe of davinci_mdio.0 failed with error -5 [ 3.750305] PPP generic driver version 2.4.2 [ 3.755096] PPP BSD Compression module registered [ 3.760009] PPP Deflate Compression module registered [ 3.765991] PPP MPPE Compression module registered [ 3.771026] NET: Registered protocol family 24 [ 3.775970] usbcore: registered new interface driver zd1201 [ 3.782043] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 3.789337] usbcore: registered new interface driver cdc_wdm [ 3.795288] Initializing USB Mass Storage driver... [ 3.800628] usbcore: registered new interface driver usb-storage [ 3.806884] USB Mass Storage support registered. [ 3.812103] usbcore: registered new interface driver usbserial [ 3.818328] USB Serial support registered for generic [ 3.823822] usbcore: registered new interface driver usbserial_generic [ 3.830657] usbserial: USB Serial Driver core [ 3.835327] USB Serial support registered for GSM modem (1-port) [ 3.841888] usbcore: registered new interface driver option [ 3.847717] option: v0.7.2:USB Driver for GSM modems [ 3.853363] mousedev: PS/2 mouse device common for all mice [ 3.860107] input: ti-tsc as /devices/platform/omap/ti_tscadc/tsc/input/input0 [ 3.868682] omap_rtc am33xx-rtc: rtc core: registered am33xx-rtc as rtc0 [ 3.875946] i2c /dev entries driver [ 3.879943] Linux video capture interface: v2.00 [ 3.885131] usbcore: registered new interface driver uvcvideo [ 3.891143] USB Video Class driver (1.1.1) [ 3.911193] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 3.922302] cpuidle: using governor ladder [ 3.927185] cpuidle: using governor menu [ 3.936462] omap4_aes_mod_init: loading AM33X AES driver [ 3.942199] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02 [ 3.948852] omap4_aes_probe: probe() done [ 3.953613] omap4_sham_mod_init: loading AM33X SHA/MD5 driver [ 3.959808] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03 [ 3.975494] omap4_sham_probe: probe() done [ 3.986114] usbcore: registered new interface driver usbhid [ 3.992004] usbhid: USB HID core driver [ 3.996765] tiadc tiadc: attached adc driver [ 4.002197] usbcore: registered new interface driver snd-usb-audio [ 4.011169] _regulator_get: 1-001b supply IOVDD not found, using dummy regulator [ 4.019012] _regulator_get: 1-001b supply DVDD not found, using dummy regulator [ 4.026824] _regulator_get: 1-001b supply AVDD not found, using dummy regulator [ 4.034576] _regulator_get: 1-001b supply DRVDD not found, using dummy regulator [ 4.045532] asoc: tlv320aic3x-hifi <-> davinci-mcasp.1 mapping ok [ 4.053588] ALSA device list: [ 4.056732] #0: AM335X EVM [ 4.059783] oprofile: hardware counters not available [ 4.065124] oprofile: using timer interrupt. [ 4.069641] Netfilter messages via NETLINK v0.30. [ 4.074707] nf_conntrack version 0.5.0 (3947 buckets, 15788 max) [ 4.081512] ctnetlink v0.93: registering with nfnetlink. [ 4.087188] NF_TPROXY: Transparent proxy support initialized, version 4.1.0 [ 4.094543] NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd. [ 4.101440] xt_time: kernel timezone is -0000 [ 4.106292] ip_tables: (C) 2000-2006 Netfilter Core Team [ 4.112182] ipt_CLUSTERIP: ClusterIP Version 0.8 loaded successfully [ 4.118927] arp_tables: (C) 2002 David S. Miller [ 4.123901] TCP cubic registered [ 4.127319] NET: Registered protocol family 17 [ 4.132019] can: controller area network core (rev 20090105 abi 8) [ 4.138641] NET: Registered protocol family 29 [ 4.143341] can: raw protocol (rev 20090105) [ 4.147827] can: broadcast manager protocol (rev 20090105 t) [ 4.153869] Registering the dns_resolver key type [ 4.158874] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 4.166992] ThumbEE CPU extension supported. [ 4.171539] mux: Failed to setup hwmod io irq -22 [ 4.177246] Power Management for AM33XX family [ 4.182189] Trying to load am335x-pm-firmware.bin (60 secs timeout) [ 4.188934] Copied the M3 firmware to UMEM [ 4.193328] Cortex M3 Firmware Version = 0x181 [ 4.203704] clock: disabling unused clocks to save power [ 4.215576] mmc1: new high speed MMC card at address 0001 [ 4.222259] mmcblk0: mmc1:0001 008G92 7.28 GiB [ 4.227325] mmcblk0boot0: mmc1:0001 008G92 partition 1 4.00 MiB [ 4.233734] mmcblk0boot1: mmc1:0001 008G92 partition 2 4.00 MiB [ 4.242126] mmcblk0: unknown partition table [ 4.249359] mmcblk0boot1: unknown partition table [ 4.257202] mmcblk0boot0: unknown partition table [ 4.267730] Detected MACID=84:eb:18:ec:ae:a1 [ 4.273529] cpsw: Detected MACID = 84:eb:18:ec:ae:a3 [ 4.279937] omap_rtc am33xx-rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800) [ 4.289642] VFS: Cannot open root device "mmcblk0p2" or unknown-block(179,2) [ 4.297119] Please append a correct "root=" boot option; here are the available partitions: [ 4.305938] b300 7634944 mmcblk0 driver: mmcblk [ 4.311584] b310 4096 mmcblk0boot1 (driver?) [ 4.317169] b308 4096 mmcblk0boot0 (driver?) [ 4.322784] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2) [ 4.331695] Backtrace: [ 4.334320] [] (dump_backtrace+0x0/0x10c) from [] (dump_stack+0x18/0x1c) [ 4.343231] r6:00008000 r5:c0582380 r4:c06e4b48 r3:c069934c [ 4.349212] [] (dump_stack+0x0/0x1c) from [] (panic+0x64/0x194) [ 4.357299] [] (panic+0x0/0x194) from [] (mount_block_root+0x174/0x228) [ 4.366088] r3:00000004 r2:00000000 r1:cf01df40 r0:c0582380 [ 4.372100] r7:c05823e8 [ 4.374755] [] (mount_block_root+0x0/0x228) from [] (mount_root+0xc8/0xe8) [ 4.383850] [] (mount_root+0x0/0xe8) from [] (prepare_namespace+0x16c/0x1c0) [ 4.393127] r4:c06e1ea0 [ 4.395782] [] (prepare_namespace+0x0/0x1c0) from [] (kernel_init+0xf4/0x120) [ 4.405151] r5:c06713e4 r4:c06713e4 [ 4.408935] [] (kernel_init+0x0/0x120) from [] (do_exit+0x0/0x65c) [ 4.417297] r5:c0633808 r4:00000000