Release notes for TMS320C6455 DSK

 

Spectrum Digital Inc                                                               

12502 Exchange Dr.

Suite 440

Stafford, Texas 77477                                 

 

Web:                http://www.spectrumdigital.com/

Support:           mailto:support@spectrumdigital.com

Phone:             281-494-4500

Fax:                 281-494-5310

 

Processor Supported:

TMS320C6455 on TMS320C6455 DSK

 

Operating Systems Supported:

Windows 2000 with service pack 2

Windows XP

 

USB Connection:

Version 1.10 or 2.0

 

Code Composer version supported:

Version 3.2

 

Product Release          3.0

Release Date               July 2006

 

2.0 Installation

See Quick Start guide shipped with product for step by step install.

 

3.0 Some Basics on How it Works

When the DSK is powered up the embedded USB controller will boot up and wait for enumeration from the host.  Once the host has enumerated, Code Composer can be started. When a USB device is enumerated it will show up under the Windows Hardware Device Manager.  When Code Composer is started the emulation driver will make contact with the DSK (see led DS201 flash).  It will then download the emulation firmware to the DSK.  Once that is complete the firmware will disconnect from the USB bus and reconnect as an emulator.  When the LED DS201 is on solid the USB controller is disconnected from the USB bus. DS201 will normally be on solid for ~1 second to meet the USB disconnect reconnect timing.  Once connected DS201 will flash during emulation activity.  When you exit Code Composer the DDB will once again disconnect from the USB bus and reconnect in boot mode, ready for the next debug session.  The C6455DSK icon is used to load the emulation app then start CCS. 

 

The USB controller is not affected by the DSK reset push-button.  When the DSK is powered on the USB controller gets a power on reset.  The USB controller does NOT pull a hardware reset on the C6455 processor or hold the C6455 in reset. This allows the DSK to run standalone.

 

To use the external emulator JTAG port, power off the DSK, install the JTAG cable and power the DSK. By default the embedded USB controller will supply JTAG signals to the C6455.  When the external JTAG cable is plugged, in the JTAG signals are switched asynchronously to the external emulator.  This can cause glitches on the C6455 JTAG signals.  With the external emulator is plugged in when power is off, the DSK will startup in external emulator mode with clean JTAG signals

 

You have to be logged on as an administrator to install USB devices on Windows 2000/XP.  Under Windows each time you move your USB cable to a new port on the same machine this is a new install. This can be annoying if you move your USB cable around to different ports.  During the install process you can cycle through installing the DSK on all your USB ports.  This "preps" your machine to run the DSK on any of its USB ports.

 

4.0 Limitations

4.0.1 Single DSK per PC

Multiple DSKs on one host are NOT supported.

 

4.027 SDSsq19464 Admin privileges needed for Code Composer Studio installation

 

Release Note
CCS requires access to specific registry entries when installing and using the tool. In certain installations of CCS, while in user mode, you are prevented from writing to the registry. The following instructions provide details of how to install CCS with Administrative privileges and allow write access in the registry as a user. 

Windows NT

The Code Composer Studio product needs to be installed using an account with Administrator privileges:

1. Log in as an administrator.
2. Install the product by running <setup.exe>.
3. If the installation process prompts for a reboot, the administrator must log in again prior to first use. This will allow the installation process to update registry settings after a reboot.

Once this procedure is complete users belonging to the "Users" group may fully utilize the Code Composer Studio product.

Windows 2000

Similar to the procedure on Windows NT, the Code Composer Studio product needs to be installed using an account with Administrator privileges. If the installation process prompts for a reboot the administrator must log in again prior to first use. This will allow the installation process to update registry settings after a reboot.

However, the "Users" account under Windows 2000 is, by default, significantly more restricted than a "Users" account under Windows NT. One of the new restrictions is that the "Users" group has read-only access to all parts of the registry. During its normal course of operation, Code Composer Studio reads and writes configuration and session information to the registry. There are two possible actions that may be taken to allow non-administrator users to use Code Composer Studio:

1. The administrator may modify registry permissions for the areas of registry that are used by Code Composer Studio. The procedure to do this is as follows:

a) Log in as an administrator.
b) Choose "Start->Run" from the Windows 2000 Start menu.
c) Type "regedt32" (not "regedit") to bring up the Registry Editor.
d) From the "Window" menu, select "HKEY_LOCAL_MACHINE on the Local Machine".
e) Expand the "SOFTWARE" key.
f) Locate and select the sub-key "GODSP".
g) With "GODSP" selected, choose "Security Permissions..." from the menu.
h) In the upper half of the "Permissions for GODSP" window there will be a list of all the users and groups that access the key.

i) Select the "Users" group.
j) In the "Permissions:" box, locate the item "Full Control" and check the corresponding box under "Allow".
k) Repeat steps "e" through "i" for "HKLM\Software\Texas Instruments."

2. The second option is to allow users that will be using the Code Composer Studio product access via a "Power User" account. "Power User" accounts on Windows 2000 provide an access level similar to that of a "User" account on WinNT.