# Each field should be seperated by a TAB character						
# The first column is the import configuration files which must be created using cc_setup						
# All the configuration files must be located in %WINDIR%\ti\drivers\import						
# The second column is a short description the user will see. This should have enough information that the advanced user will not need to read the long description						
# The short description should not be too cryptic for the novice users and no two configurations should have the same short description.						
# The long description should contain any detailed information which the user may need to know						
# Enter an asterisk in a field to mean that this field does not apply to the given configuration file						
# To save this file highlight the area you want to save, copy it to the clipboard then paste it into Notepad						
Configuration file	Short Description	Long Description	Family	Platform	Endianness	Memory Map
dsk6455_v2.ccs	        C6455 DSK	                One Spectrum Digital TMS320C645X DSK connected via USB set to i/o port 0x540.	C6455	dsk	*	*

# DSK6455 Plus Mezzanine card
dsk6455_with_mezzanine_v2.ccs	        C6455 DSK with Mezzanine	                One Spectrum Digital TMS320C645X DSK and one TMS320C645x Mezzanine card connected via USB set to i/o port 0x540.	C6455	dsk	*	*