IMPORTANT NOTICE - PLEASE READ
------------------------------------------------------------
This is a CSL 3.0 architecture release for the 6455 device.  Please note that if you have an existing CSL which is of the 2x architecture flavor then this CSL will not be compatible with that.  You are requested to pay careful attention to the API documentation in this product because this will delineate the differences between the CSL 3.0 architecture and the older 2x architecture.  At this time there is no specific migration documentation attempted to address the CSL 2x to 3.0 changes but in perusing the CSL 3.0 API documentation you will be able to detect the changes made in the API from CSL 2x to CSL 3.0. 

For all questions please email arichard@ti.com or call 011-91-80-25048073.