SRIO CSL EXAMPLE 
================
The folders in this directory contain a example that demonstrates the usage of SRIO CSL 3.x API's.

Hardware Requirement:
------------------
To run this example, adapter board ((AMC-TO-SMA SR10 board)) is required to connect to the EVM.

Directory structure:
---------------------

src - contains the example source files
inc - contains the example include files
build  - contains the example projects and the linker command file 
		

To Run the Example in the little endian mode:
---------------------------------------------

1. Choose the Little endian configuration in the CCS setup.

2. Open the Srio_ext_loopback_example.pjt in the CCS .

3. Ensure that the gel file is loaded.

4. In the project build options configure the endianness to little endian.

5. Ensure that the libraries rts64plus.lib, little endian intc (if required) and csl libraries are included.
Note: By default, the project is configured in little endian mode, so the above step may not be required

6. Build the project.

7. Load the OUTPUT file.

8. Execute. 


To Run the Example in the big endian mode:
------------------------------------------

1. Choose the Big endian configuration in the CCS setup.

2. Open the Srio_ext_loopback_example.pjt in the CCS.

3. Ensure that the gel file is loaded.

4. In the project build options configure the endianness to big endian.

5. Include the libraries rts64pluse.lib and the big endian intc (if required) and csl libraries

6. Build the project.

7. Load the OUTPUT file.

8. Execute.