Hi, Now I have some troubles with the nandboot of EVM6670l. Please check my operations carefully and help me to get the issues. Thanks. Setup software: setup_CCS_5.0.3.00028.zip bios_mcsdk_02_00_01_12_setup.exe NAND boot over I2C example A simple hua_evmc6670l example demonstrating NAND boot over I2C. Steps to build the example: 1.Import the hua_evmc6670l CCS project from C:\Program Files\Texas Instruments\mcsdk_2_00_01_12\demos\hua\evmc6670l directory. (in CCSv5, Project->Import Existing CCS/CCE Eclipse Projects) 2.Clean the hua_evmc6670l project and re-build the project, after build is completed, hua_evmc6670l.out and hua_evmc6670l.map will be generated under C:\Program Files\Texas Instruments\mcsdk_2_00_01_12\demos\hua\evmc6670l \bin directory. Steps to run hua_evmc6670l in CCSv5: 1. Be sure to set the boot mode dip switch to no boot/EMIF16 boot mode on the EVM. "No Boot" mode is: SW6 [position 4, 3, 2, 1] = On, On, On, On = 4b0000 SW5 [position 4, 3, 2, 1] = Off, On, On, On = 4b1000 SW4 [position 4, 3, 2, 1] = On, On, On, On = 4b0000 SW3 [position 4, 3, 2, 1] = On, On, On, Application specific Endianess = 4b000x (where x = off for little endian and on for big endian) 2. Make sure the pin2 of SW9 on evm6670l board is off.And setting the IP of PC as 192.168.2.101,then connecting the reticle between the board and PC . 3.Load the program C:\Program Files\Texas Instruments\mcsdk_2_00_01_12\demos\hua\evmc6670l \bin\ hua_evmc6670l.out to CCS. 4. Run the program in CCS.After that ,you can scan the Internet address of 192.168.2.100 on PC. Steps to program hua_evmc6670l to NAND: 1.Configure GEL Change C:\ProgramFiles\TexasInstruments\mcsdk_2_00_01_12\tools\boot_loader\ibl\src\make\bin\i2cConfig.gel to read: replace ibl.bootModes[1].u.nandBoot.bootFormat = ibl_BOOT_FORMAT_BBLOB; with ibl.bootModes[1].u.nandBoot.bootFormat = ibl_BOOT_FORMAT_ELF; 2. Load IBL Programing "IBL" on the EEPROM at bus address 0x51 Use the I2C EEPROM writer for c6670 EVM from the MCSDK distribution. Program C:\Program Files\Texas Instruments\mcsdk_2_00_01_12\tools\boot_loader\ibl\src\make\bin\i2crom_0x51_c6670_le.dat (IBL image) to the EEPROM at I2C BUS address 0x51 following the EEPROM writer's procedure. Rename file to app.dat Make sure eepromwriter_input.txt is set to load app.dat to I2C address 81 (0x51) Other parameters not changed: start_addr = 0 swap_data = 0 Power-down EVM Set boot pins to little endian "No Boot" Launch the EVM6670 target configuration Load the evm6670l.gel file that accompanied the CCSv5 patch Wait for memory map setup to complete Connect to Core 0 Wait for GEL initialization sequence to finish Load Core 0 with writer\eeprom\evmc66xxl\bin\eepromwriter_evm6670l.out Load memory location 0x80000000 with the app.dat file, making sure to use the header information to set the size of the memory block Run the EEPROM writer program ===Everything runs successfully 3.Configure IBL Terminate previous debug session (load IBL session) Power-down EVM Power-up EVM Boot pins still set to little endian "No Boot" Launch the EVM6670 target configuration Load the evm6670l.gel file that accompanied the CCSv5 patch Wait for memory map setup to complete Connect to Core 0 Wait for GEL initialization sequence to finish Load Core 0 with C:\Program Files\Texas Instruments\mcsdk_2_00_01_12\tools\boot_loader\ibl\src\make\bin\i2cparam_0x51_c6670_le_0x500.out Load GEL file C:\Program Files\Texas Instruments\mcsdk_2_00_01_12\tools\boot_loader\ibl\src\make\bin \i2cConfig.gel Run the i2cparam_0x51_c6670_le_0x500.out program Run the EVM c6670 IBL -> setConfig_c6670_main GEL script Press "Enter" ===Program states that the I2C table write completed 4.Program NAND Terminate previous debug session (configure IBL session) Power-down EVM Copy C:\Program Files\Texas Instruments\mcsdk_2_00_01_12\demos\hua\evmc6670l \bin\ hua_evmc6670l.out and rename it to app.bin. Power-up EVM Boot pins still set to little endian "No Boot" Launch the EVM6670 target configuration Load the evm6670l.gel file that accompanied the CCSv5 patch Wait for memory map setup to complete Connect to Core 0 Wait for GEL initialization sequence to finish Load Core 0 with C:\Program Files\Texas Instruments\mcsdk_2_00_01_12\tools\writer\nand\evmc6670l\bin \nandwriter_evm6678l.out Load memory location 0x80000000 with the app.bin file, making sure to use the header information to set the size of the memory block . Set the Start Address to "0x80000000", Type-size to 32-bits, leave swap unchecked, click "finish" Run the nandwriter_evm6670l.out program ===Console states that the NAND programing completed successfully 5.Test NAND Terminate previous debug session (program NAND session) Power-down EVM Configure boot pins for little endian NAND boot " NAND Boot: Set the dip switches (pin1, pin2, pin3, pin4) to: SW3(off, off, on, off), SW4(on, off, on, on), SW5(on, on, on, off), SW6(on, on, on, on) This will set the boot para index to 2 to boot the NAND image, by default the boot configuration table sets the NAND offset address to be 16384 (start of block 1) and image format to be BBLOB for image 0." Power-up the EVM After POR, IBL will boot the image from NAND.