Starting kernel ... Uncompressing Linux... done, booting the kernel. [ 0.000000] Linux version 3.2.0 (root@ryan-desktop) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #2 Fri May 16 19:00:14 CST 2014 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine: am335xevm [ 0.000000] Memory policy: ECC disabled, Data cache writeback [ 0.000000] AM335X ES2.1 (sgx neon ) [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext3 rootwait ip=none [ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes) [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Memory: 512MB = 512MB total [ 0.000000] Memory: 513168k/513168k available, 11120k reserved, 0K highmem [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB) [ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB) [ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB) [ 0.000000] .text : 0xc0008000 - 0xc0599000 (5700 kB) [ 0.000000] .init : 0xc0599000 - 0xc05d4000 ( 236 kB) [ 0.000000] .data : 0xc05d4000 - 0xc063e6a0 ( 426 kB) [ 0.000000] .bss : 0xc063e6c4 - 0xc066d4a4 ( 188 kB) [ 0.000000] NR_IRQS:396 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz [ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz [ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms [ 0.000000] Console: colour dummy device 80x30 [ 0.000091] Calibrating delay loop... 795.44 BogoMIPS (lpj=3977216) [ 0.038696] pid_max: default: 32768 minimum: 301 [ 0.038787] Security Framework initialized [ 0.038879] Mount-cache hash table entries: 512 [ 0.039215] CPU: Testing write buffer coherency: ok [ 0.059020] omap_hwmod: pruss: failed to hardreset [ 0.060028] print_constraints: dummy: [ 0.060333] NET: Registered protocol family 16 [ 0.062225] OMAP GPIO hardware version 0.1 [ 0.064544] omap_mux_init: Add partition: #1: core, flags: 0 [ 0.066101] am335x_mac_addr: mac_lo 5e9c, mac_hi f78cba1c [ 0.066101] am335x_mac_addr: mac_lo 609c, mac_hi f78cba1c [ 0.066101] Welcome To Portwell Technology [ 0.066131] Board name: A335X_SK [ 0.066131] Board version: 1.2B [ 0.066131] The board is a Parm-3354-EVC. [ 0.179138] omap_hsmmc.0: alias fck already exists [ 0.179351] omap_hsmmc.1: alias fck already exists [ 0.180084] da8xx_lcdc.0: alias fck already exists [ 0.180877] failed to get adapter i2c1 [ 0.180908] d_can.0: alias fck already exists [ 0.181762] _regulator_get: l3_main.0 supply vdd_core not found, using dummy regulator [ 0.181823] am335x_opp_update: physical regulator not present for core(-22) [ 0.182067] registered am33xx_sr device [ 0.182220] omap_i2c.1: alias fck already exists [ 0.183044] omap2_mcspi.1: alias fck already exists [ 0.183227] omap2_mcspi.2: alias fck already exists [ 0.184082] edma.0: alias fck already exists [ 0.184082] edma.0: alias fck already exists [ 0.184112] edma.0: alias fck already exists [ 0.208648] bio: create slab at 0 [ 0.210723] SCSI subsystem initialized [ 0.212188] usbcore: registered new interface driver usbfs [ 0.212463] usbcore: registered new interface driver hub [ 0.212646] usbcore: registered new device driver usb [ 0.212921] registerd cppi-dma Intr @ IRQ 17 [ 0.212921] Cppi41 Init Done Qmgr-base(e087a000) dma-base(e0878000) [ 0.212921] Cppi41 Init Done [ 0.212951] musb-ti81xx musb-ti81xx: musb0, board_mode=0x10, plat_mode=0x0 [ 0.213226] musb-ti81xx musb-ti81xx: musb1, board_mode=0x10, plat_mode=0x1 [ 0.214233] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz [ 0.215270] tps65910 1-002d: JTAGREVNUM 0x0 [ 0.217620] print_constraints: VRTC: [ 0.219024] print_constraints: VIO: at 1500 mV [ 0.221313] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal [ 0.223571] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal [ 0.224548] print_constraints: VDD3: 5000 mV [ 0.225921] print_constraints: VDIG1: at 1800 mV [ 0.227325] print_constraints: VDIG2: at 1800 mV [ 0.228729] print_constraints: VPLL: at 1800 mV [ 0.230133] print_constraints: VDAC: at 1800 mV [ 0.231506] print_constraints: VAUX1: at 1800 mV [ 0.232910] print_constraints: VAUX2: at 3300 mV [ 0.234313] print_constraints: VAUX33: at 3300 mV [ 0.235687] print_constraints: VMMC: at 3300 mV [ 0.236145] tps65910 1-002d: No interrupt support, no core IRQ [ 0.237457] Advanced Linux Sound Architecture Driver Version 1.0.24. [ 0.238464] Switching to clocksource gp timer [ 0.252166] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host) [ 0.252349] musb-hdrc musb-hdrc.0: dma type: dma-cppi41 [ 0.252624] MUSB0 controller's USBSS revision = 4ea20800 [ 0.252655] musb0: Enabled SW babble control [ 0.253051] musb-hdrc musb-hdrc.0: MUSB HDRC host driver [ 0.253143] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1 [ 0.253265] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 0.253295] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 0.253295] usb usb1: Product: MUSB HDRC host driver [ 0.253295] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd [ 0.253326] usb usb1: SerialNumber: musb-hdrc.0 [ 0.254028] hub 1-0:1.0: USB hub found [ 0.254058] hub 1-0:1.0: 1 port detected [ 0.254577] musb-hdrc musb-hdrc.0: USB OTG mode controller at e083c000 using DMA, IRQ 18 [ 0.254730] musb-hdrc musb-hdrc.1: dma type: dma-cppi41 [ 0.255035] MUSB1 controller's USBSS revision = 4ea20800 [ 0.255065] musb1: Enabled SW babble control [ 0.255432] musb-hdrc musb-hdrc.1: MUSB HDRC host driver [ 0.255462] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2 [ 0.255554] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002 [ 0.255584] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 0.255584] usb usb2: Product: MUSB HDRC host driver [ 0.255584] usb usb2: Manufacturer: Linux 3.2.0 musb-hcd [ 0.255615] usb usb2: SerialNumber: musb-hdrc.1 [ 0.256286] hub 2-0:1.0: USB hub found [ 0.256317] hub 2-0:1.0: 1 port detected [ 0.256835] musb-hdrc musb-hdrc.1: USB Host mode controller at e083e800 using DMA, IRQ 19 [ 0.257202] NET: Registered protocol family 2 [ 0.257385] IP route cache hash table entries: 4096 (order: 2, 16384 bytes) [ 0.257629] TCP established hash table entries: 16384 (order: 5, 131072 bytes) [ 0.257904] TCP bind hash table entries: 16384 (order: 4, 65536 bytes) [ 0.258056] TCP: Hash tables configured (established 16384 bind 16384) [ 0.258056] TCP reno registered [ 0.258087] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.258087] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.258270] NET: Registered protocol family 1 [ 0.258575] RPC: Registered named UNIX socket transport module. [ 0.258575] RPC: Registered udp transport module. [ 0.258575] RPC: Registered tcp transport module. [ 0.258605] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.258819] NetWinder Floating Point Emulator V0.97 (double precision) [ 0.276794] VFS: Disk quotas dquot_6.5.2 [ 0.276855] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.277313] msgmni has been set to 1002 [ 0.280151] alg: No test for stdrng (krng) [ 0.280792] io scheduler noop registered [ 0.280792] io scheduler deadline registered [ 0.280853] io scheduler cfq registered (default) [ 0.282501] da8xx_lcdc da8xx_lcdc.0: GLCD: Found NHD-4.3-ATXI#-T-1 panel [ 0.291076] Console: switching to colour frame buffer device 60x34 [ 0.296539] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0 [ 1.079284] console [ttyO0] enabled [ 1.083648] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1 [ 1.091522] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2 [ 1.099304] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3 [ 1.107055] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4 [ 1.114837] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5 [ 1.123077] omap4_rng omap4_rng: OMAP4 Random Number Generator ver. 2.00 [ 1.138275] brd: module loaded [ 1.145812] loop: module loaded [ 1.149322] i2c-core: driver [tsl2550] using legacy suspend method [ 1.155792] i2c-core: driver [tsl2550] using legacy resume method [ 1.163879] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.170989] omap2-nand driver initializing [ 1.175415] OneNAND driver initializing [ 1.180633] CAN device driver interface [ 1.184631] CAN bus driver for Bosch D_CAN controller 1.0 [ 1.191070] d_can d_can.0: device registered (irq=52, irq_obj=53) [ 1.239135] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 [ 1.245605] davinci_mdio davinci_mdio.0: detected phy mask fffffffc [ 1.253784] davinci_mdio.0: probed [ 1.257354] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown [ 1.264739] davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown [ 1.272491] usbcore: registered new interface driver zd1201 [ 1.278472] usbcore: registered new interface driver cdc_ether [ 1.284790] usbcore: registered new interface driver cdc_eem [ 1.290893] usbcore: registered new interface driver dm9601 [ 1.296752] cdc_ncm: 04-Aug-2011 [ 1.300292] usbcore: registered new interface driver cdc_ncm [ 1.306213] Initializing USB Mass Storage driver... [ 1.311553] usbcore: registered new interface driver usb-storage [ 1.317840] USB Mass Storage support registered. [ 1.323089] mousedev: PS/2 mouse device common for all mice [ 1.330139] input: ft5x0x_ts as /devices/virtual/input/input0 [ 1.390411] omap_rtc am33xx-rtc: rtc core: registered am33xx-rtc as rtc0 [ 1.397460] am33xx-rtc: already running [ 1.401672] i2c /dev entries driver [ 1.405700] Linux video capture interface: v2.00 [ 1.410858] usbcore: registered new interface driver uvcvideo [ 1.416870] USB Video Class driver (1.1.1) [ 1.480102] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 1.488555] cpuidle: using governor ladder [ 1.493286] cpuidle: using governor menu [ 1.501861] omap4_aes_mod_init: loading AM33X AES driver [ 1.507507] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02 [ 1.514038] omap4_aes_probe: probe() done [ 1.518432] omap4_sham_mod_init: loading AM33X SHA/MD5 driver [ 1.524597] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03 [ 1.535980] omap4_sham_probe: probe() done [ 1.542572] usbcore: registered new interface driver usbhid [ 1.548400] usbhid: USB HID core driver [ 1.554351] usbcore: registered new interface driver snd-usb-audio [ 1.564483] ALSA device list: [ 1.567596] No soundcards found. [ 1.571166] oprofile: hardware counters not available [ 1.576446] oprofile: using timer interrupt. [ 1.580932] nf_conntrack version 0.5.0 (8018 buckets, 32072 max) [ 1.587707] ip_tables: (C) 2000-2006 Netfilter Core Team [ 1.593414] TCP cubic registered [ 1.596771] NET: Registered protocol family 17 [ 1.601470] can: controller area network core (rev 20090105 abi 8) [ 1.608001] NET: Registered protocol family 29 [ 1.612670] can: raw protocol (rev 20090105) [ 1.617156] can: broadcast manager protocol (rev 20090105 t) [ 1.623107] Registering the dns_resolver key type [ 1.628112] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 1.636138] ThumbEE CPU extension supported. [ 1.640686] mux: Failed to setup hwmod io irq -22 [ 1.646179] Power Management for AM33XX family [ 1.651062] Trying to load am335x-pm-firmware.bin (60 secs timeout) [ 1.657714] Copied the M3 firmware to UMEM [ 1.662109] Cortex M3 Firmware Version = 0x181 [ 1.668487] create_regulator: VDD1: Failed to create debugfs directory [ 1.677795] smartreflex smartreflex: am33xx_sr_probe: Driver initialized [ 1.687805] file: arch/arm/mach-omap2/board-am335xevm.c, line = 1051, function: backlight_init [ 1.701507] clock: disabling unused clocks to save power [ 1.725341] Detected MACID=1c:ba:8c:f7:9c:5e [ 1.730895] cpsw: Detected MACID = 1c:ba:8c:f7:9c:60 [ 1.737701] input: gpio-keys as /devices/platform/gpio-keys/input/input1 [ 1.745391] omap_rtc am33xx-rtc: setting system clock to 2013-06-26 01:00:42 UTC (1372208442) [ 1.754821] Waiting for root device /dev/mmcblk0p2... [ 1.775390] mmc1: new high speed MMC card at address 0001 [ 1.781646] mmcblk0: mmc1:0001 SEM04G 3.68 GiB [ 1.786499] mmcblk0boot0: mmc1:0001 SEM04G partition 1 2.00 MiB [ 1.792816] mmcblk0boot1: mmc1:0001 SEM04G partition 2 2.00 MiB [ 1.800354] mmcblk0: p1 p2 [ 1.805145] mmcblk0boot1: unknown partition table [ 1.811523] mmcblk0boot0: unknown partition table [ 1.871002] EXT3-fs (mmcblk0p2): recovery required on readonly filesystem [ 1.878112] EXT3-fs (mmcblk0p2): write access will be enabled during recovery [ 1.900329] kjournald starting. Commit interval 5 seconds [ 1.906127] EXT3-fs (mmcblk0p2): recovery complete [ 1.913787] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode [ 1.921051] VFS: Mounted root (ext3 filesystem) readonly on device 179:2. [ 1.928527] Freeing init memory: 236K INIT: version 2.88 booting Starting udev Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory bootlogd. [ 4.879821] EXT3-fs (mmcblk0p2): using internal journal ALSA: Restoring mixer settings... /usr/sbin/alsactl: load_state:1686: No soundcards found... Configuring network interfaces... [ 5.440826] net eth0: CPSW phy found : id is : 0x4dd074 udhcpc (v1.20.2) started Sending discover... Sending discover... Sending discover... No lease, failing done. INIT: Entering runlevel: 5 Starting system message bus: dbus. Starting Dropbear SSH server: dropbear. Starting telnet daemon. Performing wifi calibration... rm: can't remove '/lib/firmware/ti-connectivity/wl1271-nvs.bin': No such file or directory Error: Module wl12xx_sdio is not currently loaded nl80211 not found. [ 14.887054] Disabling lock debugging due to kernel taint Starting network benchmark server: netserver. Starting syslogd/klogd: done Starting thttpd. Starting PVR Starting Lighttpd Web Server: lighttpd. 2013-06-26 01:00:56: (log.c.166) server started ERROR: could not insert 'g_mass_storage': No such device *************************************************************** *************************************************************** NOTICE: This file system contains the followin GPLv3 packages: binutils-symlinks binutils gdbserver If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** Not found test program path. Stopping Bootlog daemon: bootlogd. umount: can't umount /mnt/.psplash: Device or resource busy _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am335x-evm ttyO0 Arago 2013.05 am335x-evm ttyO0 am335x-evm login: