[ 1.647216] ThumbEE CPU extension supported. [ 1.651763] mux: Failed to setup hwmod io irq -22 [ 1.657287] Power Management for AM33XX family [ 1.662139] Trying to load am335x-pm-firmware.bin (60 secs timeout) [ 1.668823] Copied the M3 firmware to UMEM [ 1.673187] Cortex M3 Firmware Version = 0x181 [ 1.680511] create_regulator: VDD1: Failed to create debugfs directory [ 1.688873] smartreflex smartreflex: am33xx_sr_probe: Driver initialized [ 1.698852] file: arch/arm/mach-omap2/board-am335xevm.c, line = 1051, function: backlight_init [ 1.712585] clock: disabling unused clocks to save power [ 1.736450] Detected MACID=1c:ba:8c:f9:2:fd [ 1.741912] cpsw: Detected MACID = 1c:ba:8c:f9:02:ff [ 1.748687] input: gpio-keys as /devices/platform/gpio-keys/input/input1 [ 1.756378] omap_rtc am33xx-rtc: setting system clock to 2013-06-25 23:15:33 UTC (1372202133) [ 1.765808] Waiting for root device /dev/mmcblk0p2... [ 1.786285] mmc1: new high speed MMC card at address 0001 [ 1.792541] mmcblk0: mmc1:0001 SEM04G 3.68 GiB [ 1.797363] mmcblk0boot0: mmc1:0001 SEM04G partition 1 2.00 MiB [ 1.803710] mmcblk0boot1: mmc1:0001 SEM04G partition 2 2.00 MiB [ 1.811187] mmcblk0: p1 p2 [ 1.815979] mmcblk0boot1: unknown partition table [ 1.822387] mmcblk0boot0: unknown partition table [ 1.881195] EXT3-fs (mmcblk0p2): recovery required on readonly filesystem [ 1.888305] EXT3-fs (mmcblk0p2): write access will be enabled during recovery [ 1.914001] kjournald starting. Commit interval 5 seconds [ 1.919860] EXT3-fs (mmcblk0p2): recovery complete [ 1.927429] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode [ 1.934692] VFS: Mounted root (ext3 filesystem) readonly on device 179:2. [ 1.942199] Freeing init memory: 236K INIT: version 2.88 booting Starting udev [ 2.517333] scsi 0:0:0:0: Direct-Access JetFlash Transcend 32GB 8.07 PQ: 0 ANSI: 4 [ 2.892272] sd 0:0:0:0: [sda] 62939136 512-byte logical blocks: (32.2 GB/30.0 GiB) [ 3.088043] sd 0:0:0:0: [sda] Write Protect is off [ 3.190399] sd 0:0:0:0: [sda] Write cache: disabled, read cache: enabled, doesn't support DPO or FUA [ 3.654205] sda: sda1 [ 3.764465] sd 0:0:0:0: [sda] Attached SCSI removable disk Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory bootlogd. [ 5.216278] EXT3-fs (mmcblk0p2): using internal journal ALSA: Restoring mixer settings... /usr/sbin/alsactl: load_state:1686: No soundcards found... Configuring network interfaces... [ 5.775634] net eth0: CPSW phy found : id is : 0x4dd074 udhcpc (v1.20.2) started Sending discover... Sending discover... Sending discover... No lease, failing done. INIT: Entering runlevel: 5 Starting system message bus: dbus. Starting Dropbear SSH server: dropbear. Starting telnet daemon. Performing wifi calibration... rm: can't remove '/lib/firmware/ti-connectivity/wl1271-nvs.bin': No such file or directory Error: Module wl12xx_sdio is not currently loaded nl80211 not found. [ 15.223449] Disabling lock debugging due to kernel taint Starting network benchmark server: netserver. Starting syslogd/klogd: done Starting thttpd. Starting PVR Starting Lighttpd Web Server: lighttpd. 2013-06-25 23:15:46: (log.c.166) server started ERROR: could not insert 'g_mass_storage': No such device *************************************************************** *************************************************************** NOTICE: This file system contains the followin GPLv3 packages: binutils-symlinks binutils gdbserver If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** Now mount USB device Not found test program path. mount error Stopping Bootlog daemon: bootlogd. umount: can't umount /mnt/.psplash: Device or resource busy _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am335x-evm ttyO0 Arago 2013.05 am335x-evm ttyO0 am335x-evm login: