C55xx CSL Library Installation
(C) Copyright 2004 Texas Instruments Incorporated
All rights reserved worldwide.
-------------------------------------------------

Contents
--------
- ZIPFILE CONTENTS
- INSTALLATION INFORMATION
- BUGS FIXED FOR CURRENT VERSION
- CONTACTING TI


ZIPFILE CONTENTS
----------------
C55xxCSL.exe - Contains the installation program for the C55x CSL Library
Readme.txt - This file.
Releasenote.htm - Release note for version 2.31.00.9


INSTALLATION INFORMATION
------------------------
To run the TI C55xx CSL Library Installation, follow the directions below:

Windows 98, Windows NT, Windows 2000, Windows XP
1. Unzip the C55xxCSL.exe file to a temporary directory
2. Double Click the executable to launch the Install Shield Wizard
3. Answer all remaining questions presented in Install Shield dialog boxes

NOTES:
1) If you DO NOT accept the software license agreement the library WILL NOT be installed.
2) The default location to install the software is C:\Program Files\C55xxCSL, which will install the
   libraries into C:\Program Files\C55xxCSL\lib, the header files into C:\Program Files\C55xxCSL\include and
   the examples into C:\Program Files\C55xxCSL\examples.
   If CSL is installed over <CCS_Install_Dir>\bios\ , it will overwrite existing CSL
   version without taking any backup. So it is recommended that user take backup of
   <CCS_Install_Dir>\bios\ folder before installing CSL there.

BUGS FIXED FOR CURRENT VERSION
------------------------------

CSL 2.x BIOS bug fixed.
             

CONTACTING TI
-------------
Texas Instruments Incorporated
Post Office Box 655303
Dallas, Texas  75265  USA

Phone: +1(972) 644-5580
Fax: +1(214) 480-7800
Internet: dsph@ti.com
World Wide Web: http://www.ti.com/sc/support