Texas Instruments     Pin Mux Utility for ARM MPU Processors v2.5.2.0		02/04/13

R E L E A S E  N O T E S 

1. See Help > Readme menu item for an updated description of program features.

2. See revision history at bottom of this file.

3. See User's Guide on this Wiki page:

   http://processors.wiki.ti.com/index.php/Pin_Mux_Utility_for_ARM_MPU_Processors_v2

4. Supports the following devices:
   AM335x Rev 1.x, AM335x Rev 2.x
   AM3505, AM3517
   AM3703, AM3715
   AM3871, AM3872, AM3874 
   AM3892, AM3894, 
   C6A8167, C6A8168
   DM3725, DM3730
   DM8165, DM8166, DM8167, DM8168, 
   OMAP3503, OMAP3515, OMAP3525, OMAP3530

5. New pin muxing features of the AM335x Silicon Revision 2.0 and later:

       a) Enhancements to AM335x Rev 2.x provide a few new pin multiplexing options that were not 
          available on AM335x Rev 1.x.

       b) Mode1 and Mode2 signal assignments for the GPMC_CSn3 terminal are only available with 
          AM335x Rev 2.x or newer devices.

       c) Mode2 signal assignment for the LCD_HSYNC and LCD_VSYNC terminals are only available 
          with AM335x Rev 2.x or newer devices.

       d) Mode2 signal assignment for the GPMC_A9 terminal on AM335x Rev 2.x or newer devices 
          has two possible signal functions which are selected with new level of pin multiplexing 
          that is controlled with bit zero of the SMA2 register.

   For more details refer to Section 1.2 of the AM335x Technical Reference Manual.

6. You can import design state files of device type AM335X or AM335x Rev 1.x or AM335x Rev 2.x.
   Files with device type AM335x were created with a previous version of this tool.  

   If you import a file with device type AM335x, for a AM335x Rev 1.x or AM335x Rev 2.x design 
   you will see an error message saying "Errors occurred loading design file."  A log file
   will be generated.  If you look at that log file it will complain about signals in the design state 
   file that are not in the current device model.  Ignore this error message.  This happens because 
   starting with Pin Mux v2.5.1.0 the following balls are removed because the pad config registers 
   are not actually implemented in the AM335x design (Rev 1.x or 2.x)
	PORZ, OSC0_IN, OSC0_OUT, OSC1_IN, OSC1_OUT, 
	USB0_DM, USB0_DP, USB0_CE, USB0_ID, USB0_VBUS,
	USB1_DM, USB1_DP, USB1_CE, USB1_ID, USB1_VBUS,
	DDR_RESETN, DDR_CSN0, DDR_CKE, DDR_CK, DDR_NCK, DDR_CASN, DDR_RASN, DDR_WEN, DDR_BA0..DDR_BA2,
	DDR_A0..DDR_A15, DDR_ODT, DDR_D0..DDR_D15, DDR_DQM0..DDR_DQM1, DDR_DQS0, DDR_DQSN0, DDR_DQS1, 
        DDR_DQSN1,DDR_VREF, DDR_VTP,AIN0..AIN7,VREFP, VREFN

    You would then see these messages in the "PinMuxDesignState_<device type>_Load_Errors.txt" file:

    Error: Ball with location string "2 ZCE E15 - ZCZ B15 - " with Mode 0 Name "PORZ" in design file was not found in the current device model.
    Error: Ball with location string "2 ZCE W11 - ZCZ V10 - " with Mode 0 Name "OSC0_IN" in design file was not found in the current device model.
    .
    .
    .
    Error: Ball with location string "2 ZCE A9 - ZCZ B9 - " with Mode 0 Name "VREFP" in design file was not found in the current device model.
    Error: Ball with location string "2 ZCE B9 - ZCZ A9 - " with Mode 0 Name "VREFN" in design file was not found in the current device model.


7. If you import a file with device type AM335x, or AM335x Rev 1.x for a AM335x Rev 2.x design 
   you will see an error message saying "Errors occurred loading design file."  A log file
   will be generated.  If you look at that file it will complain about pin mux map locations that were "Reserved" in the AM335x Rev 1.x
   but they now contain new pin muxing options.  These cells will be set to "Not Selected" during the import.

   You would then see these messages in the "PinMuxDesignState_<device type>_Load_Errors.txt" file:

   INFO: At row 35 in GUI, Importing Mode 0 Name "GPMC_CSN3" for Mux Mode 1. "Reserved" in design file was changed to "Not Selected" to match current device model.
   INFO: At row 35 in GUI, Importing Mode 0 Name "GPMC_CSN3" for Mux Mode 2. "Reserved" in design file was changed to "Not Selected" to match current device model.
   INFO: At row 57 in GUI, Importing Mode 0 Name "LCD_VSYNC" for Mux Mode 2. "Reserved" in design file was changed to "Not Selected" to match current device model.
   INFO: At row 58 in GUI, Importing Mode 0 Name "LCD_HSYNC" for Mux Mode 2. "Reserved" in design file was changed to "Not Selected" to match current device model.


8. The generated board-dependent C header file (pinmux.h) will now contain status messages about the overall status of the design
   and any specific kinds of error that occur in your design.  

   If your design has no errors you will seee this in the generated pinmux.h file:

    /* Design Status: NO ERRORS */


   This illustrates some of the error messages that can occur in the generated pinmux.h file:
   (This was a test case where I inserted several different type of errors in the same design.)

    /* Design Status: INVALID DESIGN */
    /* Design Error: PIN MUXING CONFLICT(S) - More than one signal selected at the same device ball location. */
    /* Design Error: PKG CONFLICT(S) - A signal is selected where there is no ball for this package type. Look for RED in "Bot/Top Ball" column. */
    /* Design Error: MULTI-MUXED SIGNAL VIOLATION(S) - The same internal signal is routed to more than one ball. */
    /* Design Error: I/O SET VIOLATION(S) - A peripheral interface has a combination of selected signals that are not supported. */
    /* Please reload your design state file (*.DAT) using File -> Open -> Design and check status colors in peripheral interface grid */

    If the generated pinmux.h file: has this status:

    /* Design Status: POSSIBLY INVALID DESIGN */

    There are either MULTI-MUXED SIGNAL VIOLATION(S) or PKG CONFLICT(S).
    MULTI-MUXED SIGNAL VIOLATION(S) could be OK if you intentionally output an output-only signal to multiple ball locations.

    PKG CONFLICT(S) errors could be erroneous.  If the generated pinmux.h has this type of error, do a File -> Load -> Design 
    and scan the Pin Mux Grid in the main windows for cases where entries in the "Bot/Top Ball" column are colored RED.  For 
    the ZCE package, in the USB1 interface, signal USB1_DRVVBUS is selected by default even though there is no connection to a 
    package ball location.  You can ignore the error in this case.


    
   ****************************************************************************************
   *** The remainder of the release notes apply to all versions of the Pin Mux Utility ****
   ****************************************************************************************


9. Pin Multiplexing: Valid IO Sets and Restrictions (AM335x device only)

   The AM335x device contains many peripheral interfaces. In order to reduce package size and lower overall system cost while 
   maintaining maximum functionality, many of the AM335x terminals can multiplex up to eight signal functions. Although there 
   are many combinations of pin multiplexing that are possible, only a certain number of sets, called IO Sets, are valid due to 
   timing limitations. These valid IO Sets were carefully chosen to provide many possible application scenarios for the user.
 
   Pin Mux Utility helps a system designer select the appropriate pin-multiplexing configuration for their AM335x-based 
   product design. This Pin Mux Utility provides a way to select valid IO Sets of specific peripheral interfaces to ensure 
   the pin multiplexing configuration selected for a design only uses valid IO Sets supported by the AM335x device.

   A few IO Sets have additional restrictions not defined in the Pin Mux Utility.  These additional restrictions are described below.

   MCASP0 Interface
        Operation of MCASP0 is not supported for OPP50.

   MCASP1 Interface
        Operation of MCASP1 is not supported for OPP50.

   MMC0, MMC1, MMC2 Interfaces 
        Only Standard (STD) and High Speed (HS) modes are supported. New SDR12, SDR25, SDR50 modes as defined in SD3.0 spec 
        are not supported.

   GEMAC_CPSW Interface
        Operation of GEMAC_CPSW is not supported for OPP50.

10. Interface Status for Peripheral Interfaces with IO Sets (AM335x only). 
   IO Set Match = Signal selections match a pre-defined IO Set exactly (acceptable status)

   IO Set Subset = Signal selections are a subset of a pre-defined IO Set. (acceptable status)

   IO Set Violation = Signal selections are not contained within any pre-defined valid IO Set.
                      Operation is not guaranteed. (NOT an acceptable status)

11. Includes IO power domain voltage display and checking for peripheral interfaces that are not all using the same
   IO cell supply voltage. (AM335x only) Not checked for MISC or GLUE interfaces.

12. Includes Multi-Muxed Violation status for peripheral interfaces (for all supported devices).  This applies to cases where the same 
   internal signal is muxed to multiple ball locations.  A violation is flagged if the signal is selected at more than one ball location.
   This may be intentional and acceptable if an output-only signal needs to come out at multiple ball locations.

13. Pad Configuration Parameters.
   Input Enable parameter (IDIS or IEN).  This parameter is defaulted based on the current mux selection 
   for the pad which determines the current I/O direction (I, O or I/O).  This parameter should not need 
   to be editted in most cases.  For all signals that have I/O capability, the input enable bit will 
   default to 1 (IEN).

   However, some signals with I/O capability need to be used as output only depending on 
   how the hardware module itself is configured.  If the ball needs to be configured as output,
   the Input Enable pad configuration bit is recommended to be changed to IDIS.

   Also, most GPIO signals have I/O capability.  If used as output only, the Input Enable bit is
   recommended to be set to IDIS.   


14. Other Pad Configuration Parameters.

   Active-Mode Internal Pull defaults to a setting specified in the device model for each ball.

   Standby-Mode Internal Pull defaults to PI (pull-inhibited) for all signals.  

   Active-Mode Internal Pull and Standby-Mode Internal Pull settings may need to be editted depending on
   pull-up or pull-down resistors that are present in the schematic design.

   Standby Configuration defaults to SIG (output latched signal state) for all signals.

   Wake Up Input Enable defaults to disabled for all signals.

   These parameters need to be editted on a ball-by-ball basis.  Groups of balls can be editted 
   to the same setting together if multiple cells in Pad Config column are selected.


R E V I S I O N   H I S T O R Y
---------------------------------------------------------------------------------------------------------------
Version: v2.5.2.0                 Date: 02-04-2013       Predecessor:  v2.5.1.0
---------------------------------------------------------------------------------------------------------------

1. Added release note #5 (above)

2. Removed GPLv2 license information from generated sample C header files.

---------------------------------------------------------------------------------------------------------------
Version: v2.5.1.0                 Date: 12-18-2012       Predecessor:  v2.4.1.0
---------------------------------------------------------------------------------------------------------------

1. AM335x device now has separate selections for silicon Rev 1.x and Rev 2.x.  Separate
   device data comma separated spreadsheet (.CSV) files are used.  
   AM335x Rev 1.x changes to spreadsheet v0.91 
	The following balls are removed in v0.91 because the pad config registers are not implemented.
	PORZ, OSC0_IN, OSC0_OUT, OSC1_IN, OSC1_OUT, 
	USB0_DM, USB0_DP, USB0_CE, USB0_ID, USB0_VBUS,
	USB1_DM, USB1_DP, USB1_CE, USB1_ID, USB1_VBUS,
	DDR_RESETN, DDR_CSN0, DDR_CKE, DDR_CK, DDR_NCK, DDR_CASN, DDR_RASN, DDR_WEN, DDR_BA0..DDR_BA2,
	DDR_A0..DDR_A15, DDR_ODT, DDR_D0..DDR_D15, DDR_DQM0..DDR_DQM1, DDR_DQS0, DDR_DQSN0, DDR_DQS1, DDR_DQSN1,
	DDR_VREF, DDR_VTP,
	AIN0..AIN7
	VREFP, VREFN
	 
   AM335x Rev 2.x gets spreadsheet v2.0.0.0

2. For AM335x change configuration xml file to not convert signal names in GUI to upper case or lower case.
   Allow mixed case to show as in the data manual.

3. Changed criteria for dropping a device pad from "blank pad config register name" to "blank register offset".
   This is because am335x does not have the register name column and needs to remove device pads where the
   pad config registers are not implemented.

4. Set data grid view property AutoSizeRowsMode = AllCells.  This was because with lower case signal names
   the part of the letters that extend below the bottom line get cut off.   Fixed window resizing for the
   Interface View case.  Use Rows[0].height instead of RowTemplate.height.

5. Added support for signals having multiple interface names.  This happens if there is an additional mux control
   in the IP block.  For AM335x, there is a signal "mmc2_dat7_mux0 / rmii2_crs_dv_mux2" with an interface name of
   "MMC2 / GEMAC_CPSW".  This signal will now be included in both the MMC2 and GEMAC_CPSW interface views.
   This is required to make the IO Sets work correctly.

6. Added code to insert status msgs like this in the generated board-dependent C header file (pinmux.h)
    /* Design Status: INVALID DESIGN */
    /* Design Error: PIN MUXING CONFLICT(S) - More than one signal selected at the same device ball location. */
    /* Design Error: PKG CONFLICT(S) - A signal is selected where there is no ball for this package type. Look for RED in "Bot/Top Ball" column. */
    /* Design Error: MULTI-MUXED SIGNAL VIOLATION(S) - The same internal signal is routed to more than one ball. */
    /* Design Error: I/O SET VIOLATION(S) - A peripheral interface has a combination of selected signals that are not supported. */
    /* Please reload your design state file (*.DAT) using File -> Open -> Design and check status colors in peripheral interface grid */


---------------------------------------------------------------------------------------------------------------
Version: v2.4.1.0                 Date: 04-23-2012       Predecessor:  v2.3.1.0
---------------------------------------------------------------------------------------------------------------

1. Spreadsheet update for AM335x from v0.88 to v0.89.  IO Sets table changes only.

0.89	4/5/2012	Paul Eaves	"Updated the Notes column in the SA Power Supply Pins sheet.
                                         Removed IO Sets from the PRU GPIO signals in the IO Sets sheet.
                                         Removed IO Sets from the pr1_mii0_rxlink and pr1_mii1_rxlink signals 
                                         in the IO Sets sheet.
                                         Removed the voltage restrictions from the McASP0 and McASP1 signals 
                                         in the IO Sets sheet."

2. AM389x-C6A816x-DM816x device now has separate selections for silicon Rev 1.x and Rev 2.x.  Separate
   device data comma separated spreadsheet (.CSV) files are used.

---------------------------------------------------------------------------------------------------------------
Version: v2.3.1.0                 Date: 03-13-2012       Predecessor:  v2.3.0.0
---------------------------------------------------------------------------------------------------------------

1. Spreadsheet update for AM335x from v0.87 to v0.88.

---------------------------------------------------------------------------------------------------------------
Version: v2.3.0.0                 Date: 02-24-2012       Predecessor:  v2.2.1.0
---------------------------------------------------------------------------------------------------------------

1. Spreadsheet update for AM335x from v0.83 to v0.87.