|
MSP Gas Metering Library
|
| This structure allows to configure the Time of Flight Algorithm | |
| This structure is used by GASMETERING_runAlgorithms to return the results for Abs ToF, Delta ToD and Volume Flow Rate calculations | |
| This is the Gas Metering configuration structure. All expect a a pointer to this configuration structure. The Application will define this structure via the configuration files of the library | |
| This structure is use to provide the pointer to Gas Metering HAL functions | |
| This hanlde is initialized when calling GASMETERING_configureUltrasonicMeasurement and GASMETERING_intializeAlgorithm | |
| This structure allows the user to configure firing and capture setting | |
| This structure allows user to provide Gas Meter configuration parameters | |
| The following structure contains all status flags used by the library | |
| This structure allows user to provide System Configuration parameters |