Logo
MSP Gas Metering Library
GASMETERING_Meter_Configuration Struct Reference

This structure allows user to provide Gas Meter configuration parameters. More...

#include <gasMeteringLib.h>

Data Fields

float meterConstant
 

Detailed Description

This structure allows user to provide Gas Meter configuration parameters.

Field Documentation

float GASMETERING_Meter_Configuration::meterConstant

This constant is meter dependent and is calculated using the following formula (Area x Length) length^3


The documentation for this struct was generated from the following file: