Logo
MSP Gas Metering Library
GASMETERING_System_Configuration Struct Reference

This structure allows user to provide System Configuration parameters. More...

#include <gasMeteringLib.h>

Data Fields

GASMETERING_HFXT_freq hFXTFreq
 
bool runDiagnosticFunctions
 

Detailed Description

This structure allows user to provide System Configuration parameters.

Field Documentation

bool GASMETERING_System_Configuration::runDiagnosticFunctions

Setting this values to true will run diagnostic functions. The APIs will inform the user of any errors via the API return codes.


The documentation for this struct was generated from the following file: