MSP430 Gas Metering Library 1_10_00_11
Release Notes
Document Revision: April 26, 2017
Library provides the means to configure the internal ADC for ultrasonic captures and help to integrate it
with the application software for development of Gas Meter Ultrasonic Flow Meter applications. The library also
takes advantage of LEA module in MSP43FR5994 devices to compute ToF measurements.
This document is divided into the following sections:
The MSP430 Gas Metering Library contains the following documentation:
1_10_00_11
What's New
1_10_00_10
- Added option to leave TX high via library configuration parameter.
- Added two boolean flags to GASMETERING_handle (isLEAusedHE and isLEAusedFTC) to show if LEA was used for computation.
1_10_00_09
- Update example project to leave MOSI line high.
1_10_00_08
- Fixed JIRA bugs:
- Fixed incorrect initialization of buffer used by algorithm computation.
- Fixed incorrect LEA memory allocation to store binary pattern.
- Updated CCS and IAR projects to include custom linker file.
- Addded Sync threshold parameter in Gas Metering Configuration.
Device Support
The following families of devices are support in this release of MSP430 Gas Metering
Library:
This
is the 1_10_00_11 release of MSP430 Gas Metering Library.
- CCS v6.1.3 or later
- IAR for MSP430 v6.40.2 or later
This is library version has validated. This build has passed functional
library testing and basic system level testing.
Validation:
- Long overnight tests at room temperature
Upgrade and Compatibility Information
The examples may be built with CCS and IAR for MSP430.
Known Issues
- Break after long run (suspect this is same as the GUI issue): 1 hr with 8 Hz measurement rate and likely after 2 days with 1 Hz measurement rate
This is build 1_10_00_11 of MSP430 Gas Metering library.
Bugs and enhancement request will be tracked via Jira. To submit a bug
please use the following link Submit Bug or Enhancement request
Additional Resources
For more information, visit www.ti.com.