#define READ_COIL 01 #define READ_DI 02 #define READ_HLD_REG 03 #define READ_AI 04 #define SET_COIL 05 #define SET_HLD_REG 06 #define READ_FIFO 24 #define PROTOCOL_EXCEPTION 0x81 #define PROTOCOL_ERR 1 #define FRM_ERR 2 const unsigned char auchCRCHi[] = { 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40, 0x01, 0xC0, 0x80, 0x41, 0x01, 0xC0, 0x80, 0x41, 0x00, 0xC1, 0x81, 0x40 } ; const unsigned char auchCRCLo[] = { 0x00, 0xC0, 0xC1, 0x01, 0xC3, 0x03, 0x02, 0xC2, 0xC6, 0x06, 0x07, 0xC7, 0x05, 0xC5, 0xC4, 0x04, 0xCC, 0x0C, 0x0D, 0xCD, 0x0F, 0xCF, 0xCE, 0x0E, 0x0A, 0xCA, 0xCB, 0x0B, 0xC9, 0x09, 0x08, 0xC8, 0xD8, 0x18, 0x19, 0xD9, 0x1B, 0xDB, 0xDA, 0x1A, 0x1E, 0xDE, 0xDF, 0x1F, 0xDD, 0x1D, 0x1C, 0xDC, 0x14, 0xD4, 0xD5, 0x15, 0xD7, 0x17, 0x16, 0xD6, 0xD2, 0x12, 0x13, 0xD3, 0x11, 0xD1, 0xD0, 0x10, 0xF0, 0x30, 0x31, 0xF1, 0x33, 0xF3, 0xF2, 0x32, 0x36, 0xF6, 0xF7, 0x37, 0xF5, 0x35, 0x34, 0xF4, 0x3C, 0xFC, 0xFD, 0x3D, 0xFF, 0x3F, 0x3E, 0xFE, 0xFA, 0x3A, 0x3B, 0xFB, 0x39, 0xF9, 0xF8, 0x38, 0x28, 0xE8, 0xE9, 0x29, 0xEB, 0x2B, 0x2A, 0xEA, 0xEE, 0x2E, 0x2F, 0xEF, 0x2D, 0xED, 0xEC, 0x2C, 0xE4, 0x24, 0x25, 0xE5, 0x27, 0xE7, 0xE6, 0x26, 0x22, 0xE2, 0xE3, 0x23, 0xE1, 0x21, 0x20, 0xE0, 0xA0, 0x60, 0x61, 0xA1, 0x63, 0xA3, 0xA2, 0x62, 0x66, 0xA6, 0xA7, 0x67, 0xA5, 0x65, 0x64, 0xA4, 0x6C, 0xAC, 0xAD, 0x6D, 0xAF, 0x6F, 0x6E, 0xAE, 0xAA, 0x6A, 0x6B, 0xAB, 0x69, 0xA9, 0xA8, 0x68, 0x78, 0xB8, 0xB9, 0x79, 0xBB, 0x7B, 0x7A, 0xBA, 0xBE, 0x7E, 0x7F, 0xBF, 0x7D, 0xBD, 0xBC, 0x7C, 0xB4, 0x74, 0x75, 0xB5, 0x77, 0xB7, 0xB6, 0x76, 0x72, 0xB2, 0xB3, 0x73, 0xB1, 0x71, 0x70, 0xB0, 0x50, 0x90, 0x91, 0x51, 0x93, 0x53, 0x52, 0x92, 0x96, 0x56, 0x57, 0x97, 0x55, 0x95, 0x94, 0x54, 0x9C, 0x5C, 0x5D, 0x9D, 0x5F, 0x9F, 0x9E, 0x5E, 0x5A, 0x9A, 0x9B, 0x5B, 0x99, 0x59, 0x58, 0x98, 0x88, 0x48, 0x49, 0x89, 0x4B, 0x8B, 0x8A, 0x4A, 0x4E, 0x8E, 0x8F, 0x4F, 0x8D, 0x4D, 0x4C, 0x8C, 0x44, 0x84, 0x85, 0x45, 0x87, 0x47, 0x46, 0x86, 0x82, 0x42, 0x43, 0x83, 0x41, 0x81, 0x80, 0x40 }; const unsigned char char_tab[128]= { 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 0, 0, 0, 0, 0, 0, 0, 0x0a, 0x0b, 0x0c, 0x0d, 0x0e, 0x0f, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0x0a, 0x0b, 0x0c, 0x0d, 0x0e, 0x0f, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0 }; const unsigned char tab_char[16]= { '0', '1', '2', '3', '4', '5', '6', '7', '8', '9', 'A', 'B', 'C', 'D', 'E', 'F' }; const unsigned int bit_tab[]= { BIT0, BIT1, BIT2, BIT3, BIT4, BIT5, BIT6, BIT7, BIT8, BIT9, BITA, BITB, BITC, BITD, BITE, BITF }; unsigned short crc(unsigned char *puchMsg , unsigned short usDataLen) { unsigned char uchCRCHi = 0xFF ; /* high byte of CRC initialized */ unsigned char uchCRCLo = 0xFF ; /* low byte of CRC initialized */ unsigned uIndex ; /* will index into CRC lookup table */ while (usDataLen--) /* pass through message buffer */ { uIndex = uchCRCHi ^ *puchMsg++ ; /* calculate the CRC */ uchCRCHi = uchCRCLo ^ auchCRCHi[uIndex]; uchCRCLo = auchCRCLo[uIndex] ; } return (uchCRCHi << 8 | uchCRCLo) ; } unsigned char a2toh(unsigned char *str) { unsigned char tmp; tmp = 0; tmp = char_tab[*str]; str++; tmp = tmp*16 + char_tab[* str]; return tmp; } int get_bit( unsigned int data, int bit ) { if (bit > 16) return 0; if (data & bit_tab[bit]) return 1; else return 0; } void htoa( char *str, unsigned char num) { unsigned char tmp; tmp = num; tmp = tmp & 0xf0; tmp >>= 4; *str = tab_char [ tmp]; str++; *str = tab_char [ num & 0x0f]; } int asctortu( unsigned char *dest, unsigned char *source) { unsigned char *tmp; unsigned char i; i=0; tmp = dest; if( *source !=':') return 0; source ++; while ( *source != 0x0d) { *tmp = a2toh( source); tmp ++; source ++; source ++; i++; } source ++; if ( *source != 0x0a) return 0; else { return i; } } void rtutoascii( unsigned char *dest, unsigned char *source, int lenth) { dest ++; for ( ; lenth>0; lenth--) { htoa( dest, *source); dest++; dest++; source++; } } void rtutoasc( unsigned char *dest, unsigned char *source, int lenth) { dest ++; for ( ; lenth>0; lenth--) { htoa( dest, *source); dest++; dest++; source++; } } unsigned char lrc(unsigned char *str,int lenth) { unsigned char tmp; tmp = 0; while (lenth-- ) { tmp += *str++; } return ((unsigned char)(-((char)tmp))); } void construct_ascii_frm ( unsigned char *dst_buf, unsigned char *src_buf, unsigned char lenth) { unsigned char lrc_tmp; lrc_tmp = lrc( src_buf, lenth); *(src_buf+lenth) = lrc_tmp; lenth++; *dst_buf = ':'; rtutoascii( dst_buf,src_buf, lenth); *(dst_buf + 2 * lenth+1) = 0x0d; *(dst_buf + 2 * lenth+2) = 0x0a; } void construct_rtu_frm ( unsigned char *dst_buf,unsigned char *src_buf,unsigned char lenth) { unsigned short crc_tmp; crc_tmp = crc(src_buf, lenth); *(src_buf+lenth) = crc_tmp >> 8 ; *(src_buf+lenth+1) = crc_tmp & 0xff; lenth++; lenth++; while ( lenth--) { *dst_buf = *src_buf; dst_buf++; src_buf++; } } /*1 读取继电器状态 发送: */ int ascii_read_coil_status ( unsigned char board_adr, unsigned char *com_buf,int start_address,int lenth) { unsigned char tmp[256],tmp_lenth; tmp[0] = board_adr; tmp[1] = READ_COIL; tmp[2] = HI(start_address); tmp[3] = LOW(start_address); tmp[4] = HI(lenth); tmp[5] = LOW(lenth); tmp_lenth = 6; construct_ascii_frm (com_buf, tmp, tmp_lenth); return 18; } int rtu_read_coil_status ( unsigned char board_adr,unsigned char *com_buf,int start_address,int lenth) { unsigned char tmp[256], tmp_lenth; tmp[0] = board_adr; tmp[1] = READ_COIL; tmp[2] = HI(start_address); tmp[3] = LOW(start_address); tmp[4] = HI(lenth); tmp[5] = LOW(lenth); tmp_lenth = 6; construct_rtu_frm ( com_buf, tmp, tmp_lenth); return 8; } /* 2 读取开关量输入 发送: */ int ascii_read_input_status ( unsigned char board_adr,unsigned char *com_buf,int start_address,int lenth) { unsigned char tmp[256], tmp_lenth; tmp[0] = board_adr; tmp[1] = READ_DI; tmp[2] = HI(start_address); tmp[3] = LOW(start_address); tmp[4] = HI(lenth); tmp[5] = LOW(lenth); tmp_lenth = 6; construct_ascii_frm ( com_buf, tmp, tmp_lenth); return 18; } int rtu_read_input_status ( unsigned char board_adr,unsigned char *com_buf,int start_address,int lenth) { unsigned char tmp[256], tmp_lenth; tmp[0] = board_adr; tmp[1] = READ_DI; tmp[2] = HI(start_address); tmp[3] = LOW(start_address); tmp[4] = HI(lenth); tmp[5] = LOW(lenth); tmp_lenth = 6; construct_rtu_frm ( com_buf,tmp,tmp_lenth); return 8; } /* 3 读取保持寄存器 发送: */ int ascii_read_hldreg ( unsigned char board_adr,unsigned char *com_buf,int start_address,int lenth) { unsigned char tmp[256], tmp_lenth; tmp[0] = board_adr; tmp[1] = READ_HLD_REG; tmp[2] = HI(start_address); tmp[3] = LOW(start_address); tmp[4] = HI(lenth); tmp[5] = LOW(lenth); tmp_lenth = 6; construct_ascii_frm ( com_buf, tmp, tmp_lenth); return 18; } int rtu_read_hldreg ( unsigned char board_adr,unsigned char *com_buf,int start_address,int lenth) { unsigned char tmp[256], tmp_lenth; tmp[0] = board_adr; tmp[1] = READ_HLD_REG; tmp[2] = HI(start_address); tmp[3] = LOW(start_address); tmp[4] = HI(lenth); tmp[5] = LOW(lenth); tmp_lenth = 6; construct_rtu_frm ( com_buf,tmp,tmp_lenth); return 8; } // 4 发送读取模拟量输入 int ascii_read_anloginput( unsigned char board_adr,unsigned char *com_buf,int start_address,int lenth) { unsigned char tmp[256], tmp_lenth; tmp[0] = board_adr; tmp[1] = READ_AI; tmp[2] = HI(start_address); tmp[3] = LOW(start_address); tmp[4] = HI(lenth); tmp[5] = LOW(lenth); tmp_lenth = 6; construct_ascii_frm ( com_buf, tmp, tmp_lenth); return 18; } int rtu_read_anloginput( unsigned char board_adr,unsigned char *com_buf,int start_address,int lenth) { unsigned char tmp[256],tmp_lenth; tmp[0] = board_adr; tmp[1] = READ_AI; tmp[2] = HI(start_address); tmp[3] = LOW(start_address); tmp[4] = HI(lenth); tmp[5] = LOW(lenth); tmp_lenth = 6; construct_rtu_frm ( com_buf,tmp,tmp_lenth); return 8; } /* 5 设置继电器 发送:status =0 继电器释放 否则继电器吸合,address 为吸合的继电器编号,0为第一个继电器,依次类推 */ int ascii_set_coil ( unsigned char board_adr,unsigned char *com_buf,int start_address,int status ) { unsigned char tmp[256], tmp_lenth; tmp[0] = board_adr; tmp[1] = SET_COIL ; tmp[2] = HI(start_address); tmp[3] = LOW(start_address); if ( status ) { tmp[4] = 0xff; tmp[5] = 0; } else { tmp[4]= 0; tmp[5]= 0; } tmp_lenth = 6; construct_ascii_frm ( com_buf, tmp, tmp_lenth); return 18; } int rtu_set_coil ( unsigned char board_adr,unsigned char *com_buf,int start_address,int status ) { unsigned char tmp[256], tmp_lenth; tmp[0] = board_adr; tmp[1] = SET_COIL ; tmp[2] = HI(start_address); tmp[3] = LOW(start_address); if ( status ) { tmp[4] = 0xff; tmp[5] = 0; } else { tmp[4]= 0; tmp[5]= 0; } tmp_lenth = 6; construct_rtu_frm ( com_buf, tmp, tmp_lenth); return 8 ; } /* 6 设置保持寄存器 */ int ascii_set_hldreg( unsigned char board_adr,unsigned char *com_buf,int start_address,unsigned int value ) { unsigned char tmp[256], tmp_lenth; tmp[0] = board_adr; tmp[1] = SET_HLD_REG; tmp[2] = HI(start_address); tmp[3] = LOW(start_address); tmp[4] = HI(value); tmp[5] = LOW(value); tmp_lenth = 6; construct_ascii_frm ( com_buf, tmp, tmp_lenth); return 18; } int rtu_set_hldreg( unsigned char board_adr,unsigned char *com_buf, int start_address, unsigned int value ) { unsigned char tmp[256], tmp_lenth; tmp[0] = board_adr; tmp[1] = SET_HLD_REG; tmp[2] = HI(start_address); tmp[3] = LOW(start_address); tmp[4] = HI(value); tmp[5] = LOW(value); tmp_lenth = 6; construct_rtu_frm ( com_buf, tmp, tmp_lenth); return 8 ; } /* 7接收分析: dest_p 接收到数据指针 sourc_p 串口接收缓冲区指针 data_start_address 开始地址 */ /* RTU 接收分析 */ int rtu_data_anlys( int *dest_p, unsigned char *source_p, int data_start_address, int fr_lenth) { unsigned short crc_result, crc_tmp; unsigned char tmp1, tmp2, shift; crc_tmp = *(source_p + fr_lenth-2); // crc 第一字节 crc_tmp = crc_tmp * 256 + *( source_p+fr_lenth-1); // CRC 值 crc_result = crc(source_p, fr_lenth-2); // 计算CRC 值 if ( crc_tmp != crc_result ) // CRC 校验正确 { hld_reg[0x31]++; return -1; } switch ( *(source_p+1) ) // 功能码 { case READ_COIL: /*读取继电器状态 */ for ( tmp1=0; tmp1<*( source_p+2); tmp1++) { shift = 1; for ( tmp2=0; tmp2<8; tmp2++) { *(dest_p+data_start_address+tmp1*8+tmp2) = shift & *( source_p+3); *( source_p+3) >>= 1; } } break; case READ_DI: /*读取开关量输入*/ for ( tmp1=0; tmp1<*( source_p+2); tmp1++) { shift = 1; for (tmp2=0; tmp2<8; tmp2 ++) { *(dest_p+data_start_address+tmp1*8+tmp2) = shift & *( source_p+3); *( source_p+3)>>=1; } } break; case READ_HLD_REG: /*读取保持寄存器*/ for ( tmp1=0; tmp1<*( source_p+2); tmp1+=2) { *(dest_p + data_start_address+ tmp1/2)= *( source_p+tmp1+3)*256 + *( source_p+tmp1+4) ; } break ; case 4: /*读取模拟量输入*/ for ( tmp1=0; tmp1<*( source_p+2); tmp1+=2) { *(dest_p + data_start_address+ tmp1/2) = *( source_p+tmp1+3)*256 + *( source_p+tmp1+4) ; } break; case PROTOCOL_EXCEPTION: return -1*PROTOCOL_ERR; //break; default: return -1*PROTOCOL_ERR; // break; } return 0; } int ascii_data_anlys( int *dest_p,char *source_p,int data_start_address) { unsigned char tmp[256]; int lenth; int tmp1, tmp2; char shift; lenth = asctortu(tmp, source_p); if ( lenth==0) return -1* FRM_ERR; switch (tmp[1] ) { case READ_COIL: /*读取继电器状态 */ for ( tmp1=0; tmp1>= 1; } } break; case READ_DI: /*读取开关量输入*/ for ( tmp1=0; tmp1>=1; } } break; case READ_HLD_REG: /*读取保持寄存器*/ for (tmp1=0; tmp1