/*==================================================================================*/ /* User specific Linker command file for running from FLASH */ /*==================================================================================*/ /* FILE: F28035_FLASH_{ProjectName}.CMD */ /* */ /* Description: Linker command file for User custom sections targetted to run */ /* from FLASH. */ /* */ /* Target: TMS320F28035 */ /* */ /* Version: 1.00 */ /* */ /*----------------------------------------------------------------------------------*/ /* Copyright Texas Instruments 2009 */ /*----------------------------------------------------------------------------------*/ /* Revision History: */ /*----------------------------------------------------------------------------------*/ /* Date | Description */ /*----------------------------------------------------------------------------------*/ /* 4/13/09 | Release 1.0 New release. */ /*----------------------------------------------------------------------------------*/ /* Define the memory block start/length for the F28035 PAGE 0 will be used to organize program sections PAGE 1 will be used to organize data sections Notes: Memory blocks on F2803x are uniform (ie same physical memory) in both PAGE 0 and PAGE 1. That is the same memory region should not be defined for both PAGE 0 and PAGE 1. Doing so will result in corruption of program and/or data. L0 memory block is mirrored - that is it can be accessed in high memory or low memory. For simplicity only one instance is used in this linker file. Contiguous SARAM memory blocks or flash sectors can be be combined if required to create a larger memory block. */ _Cla1Prog_Start = _Cla1funcsRunStart; --undef_sym=__cla_scratchpad_end --undef_sym=__cla_scratchpad_start MEMORY { /*Program Space*/ PAGE 0: RAML0 : origin = 0x008000, length = 0x000800 /* on-chip RAM (L0)*/ RAML3 : origin = 0x009000, length = 0x001000 /* data RAM (L3) */ OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */ FLASHH : origin = 0x3E8000, length = 0x002000 /* on-chip FLASH */ FLASHG : origin = 0x3EA000, length = 0x002000 /* on-chip FLASH */ FLASHF : origin = 0x3EC000, length = 0x002000 /* on-chip FLASH */ FLASHE : origin = 0x3EE000, length = 0x002000 /* on-chip FLASH */ FLASHD : origin = 0x3F0000, length = 0x001000 /* on-chip FLASH */ FLASHC : origin = 0x3F1000, length = 0x001000 /* on-chip FLASH */ FLASHA : origin = 0x3F3000, length = 0x004F80 /* on-chip FLASH */ CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */ BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */ CSM_PWL : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */ IQTABLES : origin = 0x3FE000, length = 0x000B50 /* IQ Math Tables in Boot ROM */ IQTABLES2 : origin = 0x3FEB50, length = 0x00008C /* IQ Math Tables in Boot ROM */ IQTABLES3 : origin = 0x3FEBDC, length = 0x0000AA /* IQ Math Tables in Boot ROM */ BOOTROM : origin = 0x3FF27C, length = 0x000D44 /* Boot ROM */ RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */ VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */ /*Data Space*/ PAGE 1 : BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */ RAMM0 : origin = 0x000050, length = 0x000300 /* on-chip RAM block M0 */ RAMM1 : origin = 0x000350, length = 0x000500 /* on-chip RAM block M1 */ CLARAM0 : origin = 0x008850, length = 0x000350 /* on-chip RAM block L1 */ CLARAM1 : origin = 0x008C00, length = 0x000400 /* on-chip RAM block L2 */ CLA_CPU_MSGRAM : origin = 0x001480, length = 0x000080 /* CLA-R/W, CPU-R message RAM */ CPU_CLA_MSGRAM : origin = 0x001500, length = 0x000080 /* CPU-R/W, CLA-R message RAM */ FLASHB : origin = 0x3F2000, length = 0x001000 /* on-chip FLASH */ } SECTIONS { /* Allocate program areas: */ .cinit : > FLASHA, PAGE = 0 .pinit : > FLASHA, PAGE = 0 .text : > FLASHA, PAGE = 0 codestart : > BEGIN PAGE = 0 ramfuncs : LOAD = FLASHD, RUN = RAML0, LOAD_START(_RamfuncsLoadStart), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), PAGE = 0 .bss_cla : > CLARAM1, PAGE = 1 Cla1Prog : LOAD = FLASHC, /* Note for running from RAM the load and RUN can be the same */ RUN = RAML3, LOAD_START(_Cla1funcsLoadStart), LOAD_END(_Cla1funcsLoadEnd), RUN_START(_Cla1funcsRunStart), PAGE = 0 csmpasswds : > CSM_PWL PAGE = 0 csm_rsvd : > CSM_RSVD PAGE = 0 /* Allocate uninitalized data sections: */ .stack : > RAMM0, PAGE = 1 .ebss : > RAMM1, PAGE = 1 .esysmem : > RAMM1, PAGE = 1 /* Initalized sections go in Flash */ /* For SDFlash to program these, they must be allocated to page 0 */ .econst : > FLASHA PAGE = 0 .switch : > FLASHA PAGE = 0 /* Allocate IQ math areas: */ IQmath : > FLASHD PAGE = 0 /* Math Code */ IQmathTables : > IQTABLES PAGE = 0, TYPE = NOLOAD /* Math Tables In ROM */ Cla1ToCpuMsgRAM : > CLA_CPU_MSGRAM PAGE = 1 CpuToCla1MsgRAM : > CPU_CLA_MSGRAM PAGE = 1 ClaDataRam0 : > CLARAM0, PAGE = 1 ClaDataRam1 : > CLARAM1, PAGE = 1 CLAmathTables : > CLARAM1, PAGE = 1 CLA1mathTables : > CLARAM1, PAGE = 1 // // Must be allocated to memory the CLA has write access to // CLAscratch : { *.obj(CLAscratch) . += CLA_SCRATCHPAD_SIZE; *.obj(CLAscratch_end) } > CLARAM0, PAGE = 1 .reset : > RESET, PAGE = 0, TYPE = DSECT vectors : > VECTORS PAGE = 0, TYPE = DSECT /* Uncomment the section below if calling the IQNexp() or IQexp() functions from the IQMath.lib library in order to utilize the relevant IQ Math table in Boot ROM (This saves space and Boot ROM is 1 wait-state). If this section is not uncommented, IQmathTables2 will be loaded into other memory (SARAM, Flash, etc.) and will take up space, but 0 wait-state is possible. */ /* IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD { IQmath.lib (IQmathTablesRam) } */ /* Uncomment the section below if calling the IQNasin() or IQasin() functions from the IQMath.lib library in order to utilize the relevant IQ Math table in Boot ROM (This saves space and Boot ROM is 1 wait-state). If this section is not uncommented, IQmathTables2 will be loaded into other memory (SARAM, Flash, etc.) and will take up space, but 0 wait-state is possible. */ /* IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD { IQmath.lib (IQmathTablesRam) } */ }