// TI File $Revision: /main/1 $ // Checkin $Date: May 27, 2009 13:04:36 $ //########################################################################### // // FILE: Example_2823xAdc.c // // TITLE: DSP2823x ADC Example Program. // // ASSUMPTIONS: // // This program requires the DSP2823x header files. // // Make sure the CPU clock speed is properly defined in // DSP2833x_examples.h before compiling this example. // // Connect signals to be converted to A2 and A3. // // As supplied, this project is configured for "boot to SARAM" // operation. The 2823x Boot Mode table is shown below. // For information on configuring the boot mode of an eZdsp, // please refer to the documentation included with the eZdsp, // // $Boot_Table: // // GPIO87 GPIO86 GPIO85 GPIO84 // XA15 XA14 XA13 XA12 // PU PU PU PU // ========================================== // 1 1 1 1 Jump to Flash // 1 1 1 0 SCI-A boot // 1 1 0 1 SPI-A boot // 1 1 0 0 I2C-A boot // 1 0 1 1 eCAN-A boot // 1 0 1 0 McBSP-A boot // 1 0 0 1 Jump to XINTF x16 // 1 0 0 0 Jump to XINTF x32 // 0 1 1 1 Jump to OTP // 0 1 1 0 Parallel GPIO I/O boot // 0 1 0 1 Parallel XINTF boot // 0 1 0 0 Jump to SARAM <- "boot to SARAM" // 0 0 1 1 Branch to check boot mode // 0 0 1 0 Boot to flash, bypass ADC cal // 0 0 0 1 Boot to SARAM, bypass ADC cal // 0 0 0 0 Boot to SCI-A, bypass ADC cal // Boot_Table_End$ // // DESCRIPTION: // // This example sets up the PLL in x10/2 mode. // // For 150 MHz devices (default) // divides SYSCLKOUT by six to reach a 25.0Mhz HSPCLK // (assuming a 30Mhz XCLKIN). // // For 100 MHz devices: // divides SYSCLKOUT by four to reach a 25.0Mhz HSPCLK // (assuming a 20Mhz XCLKIN). // // Interrupts are enabled and the ePWM1 is setup to generate a periodic // ADC SOC on SEQ1. Two channels are converted, ADCINA3 and ADCINA2. // // Watch Variables: // // Voltage1[10] Last 10 ADCRESULT0 values // Voltage2[10] Last 10 ADCRESULT1 values // ConversionCount Current result number 0-9 // LoopCount Idle loop counter // // //########################################################################### // // Original Author: D.F. // // $TI Release: 2833x/2823x Header Files V1.32 $ // $Release Date: June 28, 2010 $ //########################################################################### #include "DSP28x_Project.h" // Device Headerfile and Examples Include File #include "DSP2833x_DMA.h" // DMA Defines #define BUF_SIZE 1024 // Sample buffer size #pragma DATA_SECTION(DMABuf1,"DMARAML4"); #pragma DATA_SECTION(DMABuf2,"DMARAML5"); volatile Uint16 DMABuf1[1024]; volatile Uint16 DMABuf2[1024]; volatile Uint16 *DMADest; volatile Uint16 *DMASource; interrupt void local_DINTCH1_ISR(void); // Prototype statements for functions found within this file. interrupt void adc_isr(void); // Global variables used in this example: Uint16 LoopCount; Uint16 ConversionCount; Uint16 Voltage1[10]; Uint16 Voltage2[10]; //struct MODE_BITS modadma; main() { Uint16 i; // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the DSP2833x_SysCtrl.c file. InitSysCtrl(); EALLOW; #if (CPU_FRQ_150MHZ) // Default - 150 MHz SYSCLKOUT #define ADC_MODCLK 0x3 // HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 150/(2*3) = 25.0 MHz #endif #if (CPU_FRQ_100MHZ) #define ADC_MODCLK 0x2 // HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 100/(2*2) = 25.0 MHz #endif EDIS; // Step 2. Initialize GPIO: // This example function is found in the DSP2833x_Gpio.c file and // illustrates how to set the GPIO to it's default state. // InitGpio(); // Skipped for this example // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the DSP2833x_PieCtrl.c file. InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in DSP2833x_DefaultIsr.c. // This function is found in DSP2833x_PieVect.c. InitPieVectTable(); // Interrupts that are used in this example are re-mapped to // ISR functions found within this file. EALLOW; // This is needed to write to EALLOW protected register PieVectTable.ADCINT = &adc_isr; PieVectTable.DINTCH1= &local_DINTCH1_ISR; EDIS; // This is needed to disable write to EALLOW protected registers // Step 4. Initialize all the Device Peripherals: // This function is found in DSP2833x_InitPeripherals.c // InitPeripherals(); // Not required for this example InitAdc(); // For this example, init the ADC // Initialize DMA DMAInitialize(); // Enable ADCINT in PIE PieCtrlRegs.PIEIER1.bit.INTx6 = 1; PieCtrlRegs.PIEIER7.bit.INTx1 = 1; // IER |= M_INT1; // Enable CPU Interrupt 1 // IER |= M_INT7; //Enable INT7 (7.1 DMA Ch1) EnableInterrupts(); IER =0x41; EINT; // Enable Global interrupt INTM ERTM; // Enable Global realtime interrupt DBGM // Configure ADC AdcRegs.ADCMAXCONV.bit.MAX_CONV1 = 0x1; // Setup 2 conv's on SEQ1 AdcRegs.ADCTRL1.bit.SEQ_CASC=1; AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x3; // Setup ADCINA3 as 1st SEQ1 conv. AdcRegs.ADCCHSELSEQ1.bit.CONV01 = 0x2; // Setup ADCINA2 as 2nd SEQ1 conv. AdcRegs.ADCTRL1.bit.CONT_RUN=0; AdcRegs.ADCTRL2.bit.EPWM_SOCA_SEQ1 = 1;// Enable SOCA from ePWM to start SEQ1 AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 1; // Enable SEQ1 interrupt (every EOS) AdcRegs.ADCST.bit.INT_SEQ1 = 1; // Assumes ePWM1 clock is already enabled in InitSysCtrl(); EPwm1Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group EPwm1Regs.ETSEL.bit.SOCASEL = 4; // Select SOC from from CPMA on upcount EPwm1Regs.ETPS.bit.SOCAPRD = 3; // Generate pulse on 1st event EPwm1Regs.CMPA.half.CMPA = 0x0080; // Set compare A value EPwm1Regs.TBPRD = 0xFFFF; // Set period for ePWM1 EPwm1Regs.TBCTL.bit.CTRMODE = 0; // count up and start EPwm1Regs.ETSEL.bit.SOCAEN=1; // Configure DMA Channel DMADest = &DMABuf1[0]; DMASource = &AdcMirror.ADCRESULT0; DMACH1AddrConfig(DMADest,DMASource); DMACH1BurstConfig(15,1,1); //Will set up to use 32-bit datasize, pointers are based on 16-bit words DMACH1TransferConfig(15,1,1); //so need to increment by 2 to grab the correct location DMACH1WrapConfig(100,100,100,100); //Use timer0 to start the x-fer. //Since this is a static copy use one shot mode, so only one trigger is needed //Also using 32-bit mode to decrease x-fer time DMACH1ModeConfig(18,PERINT_ENABLE,ONESHOT_ENABLE,CONT_ENABLE,SYNC_ENABLE,SYNC_DST,OVRFLOW_DISABLE,THIRTYTWO_BIT,CHINT_END,CHINT_ENABLE); asm(" NOP"); StartDMACH1(); for(;;); } interrupt void adc_isr(void) { Voltage1[ConversionCount] = AdcRegs.ADCRESULT0 >>4; Voltage2[ConversionCount] = AdcRegs.ADCRESULT1 >>4; // Reinitialize for next ADC sequence AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1; // Reset SEQ1 AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1; // Clear INT SEQ1 bit PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE // DmaRegs.CH1.CONTROL.bit.PERINTFRC=1; return; } // INT7.1 interrupt void local_DINTCH1_ISR(void) // DMA Channel 1 { // To receive more interrupts from this PIE group, acknowledge this interrupt PieCtrlRegs.PIEACK.all = PIEACK_GROUP7; // Next two lines for debug only to halt the processor here // Remove after inserting ISR Code asm (" ESTOP0"); for(;;); }