======= before write: reg=0x00, len=1 read[0] = 0x00 ======= to reg: reg=0x00, len=1 write[0] = 0x00 ======= after write: reg=0x00, len=1 read[0] = 0x00 +++++++++++++++++++++++++++++++++++++ ON_OFF_CONFIG 1b mode 21 temper[0] = 0xAC temper[1] = 0xE2 VID=0x0017, buf: 17, 00 +++++++++++++++++++++++++++++++++++++ ======= before write: reg=0x21, len=2 read[0] = 0x17 read[1] = 0x00 ======= to reg: reg=0x21, len=2 write[0] = 0x17 write[1] = 0x00 ======= after write: reg=0x21, len=2 read[0] = 0x17 read[1] = 0x00 +++++++++++++++++++++++++++++++++++++ +++++++++++++++++++++++++++++++++++++ ======= before write: reg=0x01, len=1 read[0] = 0x80 ======= to reg: reg=0x01, len=1 write[0] = 0x80 ======= after write: reg=0x01, len=1 read[0] = 0x80 +++++++++++++++++++++++++++++++++++++ status_byte: not providing power to VOUT: 41 status_byte: Unclassified fault (e.g., UVF, OCW; check other status registers) status_word: value: 0x1841 (Bytes: 0x41 0x18) status_word: MFR bit warning status_word: Power NOT good (AVR_RDY/BVR_RDY pin is LOW) status_word: Not providing power to VOUT status_word: Unclassified fault detected MFR_SPECIFIC_STATUS: 0x40 - Bit6 (VSNS_OPEN): VSNS pin open detected (latched) vout[0] = 0x00 vout[1] = 0x00