This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教一个运放输入信号电压大于运放供电电压的事儿,关于TIDA-00879应用疑问

Other Parts Discussed in Thread: TIDA-00879, OPA333, MSP430F2274

问一个问题,我认为 运算放大器的输入端的信号电压都应该小于该运放的供电电压,只有这样,我认为,才会有R-R型运放,是吧?
但是,我在参考,学习,TIDA-00879应用范例的时候,忽然发现(难道是我计算错误?)该应用的原理图中的AFE前端运放对60V电压(600mV,60mV我还可以理解,毕竟信号电压小么,所以,输入到MSP430的SD24ADC上没有超出MSP430的AVCC供电电压)处理的时候,我计算出的结果是:输入到MSP430 SD24 ADC引脚上的电压,差分是:0.0545V,而SD24 每一个引脚对GND的电压却是60V和59.5V,也就是:IN+ = 60V,IN- = 59.5V,而,这个应用的本质是通过两个运放产生的电压作为差分电压输入到MSP430的运放的IN+和IN-上面,然后SD24对MSP430的运放进行采集量化。

我的问题是:
我是不是计算错误了?60V,59,5V?这不会搞坏MSP430芯片吧?
运算放大器的差分输入,可以向TIDA-00879 AFE模拟前段这么使用?我如果不用MSP430芯片,相反,我用OPA333外接成差分输入转单端输出的形式,是不是也可以在外接其他形式的ADC也可以啊?比如:外接MSP430F2274或者是TLV549?

我主要是不明白,为什么IN+和IN-的电压可以大于运放的供电电压。