This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA549的E/S使能管脚问题

Other Parts Discussed in Thread: OPA549, OPA548

TI的各位,你们好!

目前正在使用OPA549做一个电源,使用12V的单电源供电。

当设置9V输出时,带载0.1A~2A时,E/S脚不能拉高,大概0.5V到0V之间一直震荡,(E/S使能脚使用MCU的IO口上拉);如果不带载,先输出9V,可以拉高E/S管脚。这个问题该怎么解决?(想带载之后再拉高E/S)

  • TI的各位,你们好!

    目前正在使用OPA549做一个电源,使用12V的单电源供电。

    1.当设置9V输出时,带载0.1A~2A时,E/S脚不能拉高,大概0.5V到0V之间一直震荡,(E/S使能脚使用MCU的IO口上拉);如果不带载,先输出9V,可以拉高E/S管脚。这个问题该怎么解决?(想带载之后再拉高E/S)

  • 不拉高E/S引脚, OPA548不能输出,输出disable. 

    OPA549正常工作,E/S悬空,或者给高电平(>2.4V).

  • 我先设置输出9V,带载2A,然后控制E/S的时候不能拉高,它不能正常输出;

    但是我先设置输出9V,不带载,然后能控制E/S拉高,再加上负载,它可以正常输出。

    也就是说我先带上负载的话就不能拉高E/S,这个问题该怎么解决?