This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教一个关于求差电路的问题

设计如下一个求差电路(放大器型号为AD8021):输入信号(TP5)范围为0.6~2.6V,经过如下求差电路(Av=-1.68,ref=1.56V)后,将输入端信号转换为(3.2~0V),供12bit ADC采样。

问题如下:输入端电压小于1.34V时,输出恒定不变(饱和)。当输入电压大于1.34V时,电压由1.9V开始逐渐减小,输入电压为2.5V左右时,输出为0V。即设计输入、输出范围为0.6V~2.6V对应3.2V~0V,实际测试数据为:输入1.34V~2.5V对应输出1.9V~0V。