Differential Input Voltage Range Equal to Maximum-Rated Supply Voltage: − Non-V Devices . . . ±26 V − V-Suffix Devices... ±32 V
请问下这个正负26V是什么意思?,怎么用的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Differential Input Voltage Range Equal to Maximum-Rated Supply Voltage: − Non-V Devices . . . ±26 V − V-Suffix Devices... ±32 V
请问下这个正负26V是什么意思?,怎么用的?
后缀不带V版本的,供电电压范围为+-26V,那么差分输入电压范围Vid也能达到供电电压值。
同样,后缀带V版本的,供电电压范围+-32V,那么差分输入电压范围Vid也是能达到+-32V。
请问这个负电压输入是什么意思,就是由负电压输入吗?在GND之下吗?没太理解这个输入范围,能帮忙讲解吗?谢谢!
这个指的是双电源供电,+-26V范围,那么差分输入电压也 能达到电源轨的意思。单电源供电的话,即为0~52V供电。
如果IN-是0V,那么IN+最大电压为52V。