This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8551和XTR116芯片输出4-20ma电流环电路输出不受控

Other Parts Discussed in Thread: XTR116, DAC8551

通过官网参考电路电路图设计4-20ma电流环路输出,使用DAC8551和XTR116芯片,电路图如下:

现在通过SPI控制DAC8551输出电压VOUT能够正常变化,但是测量XTR116的VREF基准电压输出端电压为2.5V,电流输出端始终为电流输出最小值,并不随着DAC8551输出电压的变化而变化(PS:参考电路中给出的XTR116的VREF基准电压为4.096V)

请各位大神帮忙分析一下,是芯片出了问题,还是电路设计出了问题,非常感谢

  • Vref是输出引脚,Vref和Vreg可以给外部电路供电。正常情况下XTR116的Vref输出4.096V。 如果这个引脚输出不正常的话,建议是先断开外围电路,给XTR116上电,看Vref和Vreg是否输出正常。
    其次就是在您的电路中,没看到官网上参考电路的晶体管Q1,它的作用就是主要控制着满量幅的电流输出。
  • 之前对官网的电路图理解不太深,通过你的说明再结合官网的电路图可不可以这样理解:XTR116是由7脚V+作为电路的供电端,VREF和VREG都是由XTR116对外输出,由XTR116的VREG输出的5V给DAC8551的VDD引脚供电,由XTR116的VREF输出的基准电压给DAC8551的VREF引脚,无需给XTR116的VREG和DAC8551的VDD引脚进行外部供电?

    根据上述理解重新修改了电路,按这样连接是否正确?

    电路右边不全,见附件,有晶体管Q1

  • 是的,您的理解没问题,Vref可以给DAC做参考。Vreg可以给DAC供电。
    还需要注意的是,输入部分的回流是参考的Iret这个引脚的,我看DAC的GND接在了XTR116的Iret上,应该是没问题的。
    您再验证下是否得到正常输出?
  • 非常感谢!现在测量XTR116的VREF基准电压输出端电压为4.12V,但是XTR116的电流输出端还是没有电流输出;不知道是否为电流输出环路的电路影响?或者是其他问题?
  • 想再跟您了解下晶体管Q1的作用?它能否正常工作是会影响电流输出的有无,还是会使电流输出有误差?如果Q1不能正常工作,可能是电路中哪个环节产生的影响呢?谢谢