This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA227做电压跟随器的疑惑

Other Parts Discussed in Thread: OPA277, OPA227

我仿真了两个芯片,高阻抗的信号源,频率是50k的正弦波,无直流偏置,两个运放做跟随器差别这么大?

我要采集的是一个高阻抗弱信号,这个图说明OPA277更适合对吗?但是OPA277的失调电压似乎大点

  • 你的信号源阻抗很大, 需要考虑运放的输入阻抗和偏置电流的影响
  • OPA227同样也是单位增益稳定,并不是OPA227 不适合,跟输入端串联电阻R1值大小有关,或者您直接测量下OPA227的同相输入端,由于运放输入偏置电流的影响,同相端电压已经降到638mV左右了,所以输出跟随也是这个电压值。

    要么您就按照我这种方法,给偏置电流提供一个直流路径,然后跟随。

  • 当信号源是高阻抗的时候,要考虑运放的输入阻抗,输入阻抗太低会形成一个分压器的效果,对测量产生很大影响,例如用于测量PH值的运放LMC4682,输入阻抗达到10TΩ。输入偏置电流也会产生影响,2.5nA的偏置电流在1MΩ的电阻上产生2.5mV的压降,而像LMC4682的输入偏置电流只有20fA,同样情况产生的电压只有20nV。

    输入偏置电流较低的运放像JFET或者CMOS型的输入偏置电流一般都只有几十pA,或许会适合您的应用。
  • 有两个原因,OPA227的输入阻抗小,同时输入偏置电流较大。