This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lm158做电压跟随器 信号失真

Other Parts Discussed in Thread: LM158, OPA37

大家好,现在问题是这样的,一个幅值为正负12V, 频率为10KHz的双极方波经过电压跟随器后信号波形发生改变,方波信号的前后沿均变缓,在正电压部分幅值下降到非常小。电压跟随器采用LM158芯片构成,接地电阻试过10K以及不接电阻,不接地都试过。但是输出波形还是由方波变成了三角波。请问这是什么原因呢? LM158的带宽足够大:Unity-Gain Bandwidth of 1.2 MHz(运算放大器接的是正负电源) 

谢谢

电压跟随器电路图

电压跟随器输出信号(输入信号为方波)

  • LM158是一款低速放大器,受输出压摆率的限制,方波变成了三角波。如果换成OPA37等45M以上运放,基本就可以实现方波放大了。

  • 您好,

    LM158运放±5V供电,输入±12V信号是不满足输入信号范围的,并且LM158也不是轨至轨输出运放。LM158的SR是0.5V/us,如果增益是1,输出±12V,压摆率SR=24V*2*π*10KHZ/106次幂=1.508V/us,压摆率也不满足要求。
  •  您好,首先感谢您的解答。  还想请问一下,LM158双电源供电只能±5V供电吗?芯片数据手册的供电电压的范围更高(见下图1)。  LM158芯片数据手册的压摆率为0.5(见下图2),和芯片说明为0.3(见下图3)不一样。那么看其他芯片的时候应该以哪个为准呢。  谢谢!

  • 不好意思,我说的是:LM158运放在±5V供电时,输入±12V信号是不满足输入信号范围的。如数据手册所示,LM158双电源供电范围是最大为±16V; LM158压摆率B Version是0.5V/us,A Version是0.3V/us,这两种压摆率都不满足单位增益时输出±12V幅值的要求。