This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

pga308的应用问题,为何输出没有放大?

Other Parts Discussed in Thread: PGA308

最近使用pga308做开发,按照手册设计了电路,原理图如下;使用USB DAQ板和EVM软件对308进行配置,通信也正常,没有超时情况,但是不论放大倍数设置多少,始终没有放大,例如:将coarse offset设为0V,Front-End放大倍数设100倍,Fine offset设为2.5V,后两级放大分别设为0.5倍和2倍,输入用恒压源加10mv电,用示波器测输出始终为2.5V左右,改变输入输出始终不变,但是将Fine offset设为1V,1.5V等则输出会进行相应变化,请问各位大神是什么原因?谢谢

  • PGA308输入范围为0.2~Vcc-1.4V,超出这个范围;IC都不会放大。

  • 您好,两点建议:
    1) check sum是否是正确的? 在PGA308的应用手册上介绍:Correct checksum must be computed and entered by user for PGA308 in order to operate properly: www.ti.com/.../sbou069b.pdf

    2) 更换一颗PGA308再试试呢?因为即使invalid checksum或者Vout disable, 那么输出不会有信号,这里输出随输入不变,所以建议也更换一颗IC 试试。
  • 您好,目前是这样的状况,我将1W和GND分别接EVM的1W和GND,编程后,设置了100倍放大和2V偏置,但是输出只在我设置后的几秒内正常,之后就保持2V不动了,只有将两个输出接到EVM的两个ADS2上,输出才正常;另外,将配置好的参数写入OPT后,也是如此,只在上电后的几秒内输出正常,之后就在2V不动,请问是什么原因?谢谢。
  • 您好,目前是这样的状况,我将1W和GND分别接EVM的1W和GND,编程后,设置了100倍放大和2V偏置,但是输出只在我设置后的几秒内正常,之后就保持2V不动了,只有将两个输出接到EVM的两个ADS2上,输出才正常;另外,将配置好的参数写入OPT后,也是如此,只在上电后的几秒内输出正常,之后就在2V不动,请问是什么原因?谢谢。
  • 最近用308做设计时,出现了以下问题:原理图如下,之前Vsj处的电容为0.1uF,一直没有输出,之后因为没找到47pF电容,所以临时用50pF代替,至少有输出了,我将1W和GND分别接EVM的1W和GND,编程后,设置了100倍放大和2V偏置,但是输出只在我设置后的几秒内正常,之后就保持2V不动了,只有将两个输入接到EVM的两个ADS2上,输出才正常;另外,将配置好的参数写入OPT后,也是如此,只在上电后的几秒内输出正常,之后输出会突然产生一个向上的跳变,之后无论如何改变输入,都保持在我设置的2V不动,请问是什么原因?谢谢各位。

  • 不好意思,刚刚打错字了,应该是将两个输入接到EVM的两个ADS2上,我之前将Vsj的电容接0.1uF,直接没有输出,后来用50pF临时代替47pF,至少有输出了,但是除非输入接EVM的两个ADS2上,否则输出只稳定一段时间,后面就保持不动了;写入到OTP后也是如此,输入接到EVM的2个ADS2上,输出就正常,不接的话,只正常输出几秒,之后会有一个向上的跳变,然后稳定不动了,请指教,谢谢。
  • 您使用的是PGA308的EVM是吗? 我想您应该是jumper设置的不对,检查下Jumper 6,Jumper9 和Jumper 10的配置,这几个jumper主要是输入是否和ADC正确连接。
  • 您好,我是自己设计的板子,使用EVM与校准软件进行通信,只有将传感器输出经过EVM板的ADS2再接入我设计308的输入时,我设计308的输出才正常,如果不经过EVM板的两个ADS2,直接接入我设计的308的输入,则只有输出,但是没有进行放大;写入OTP后,只在上电后的几秒内输出正常,之后有输出但没放大,请问是什么原因?谢谢!

  • 问题已解决,原因是没有共地,处于浮地状态,没有产生共模电压。

  • 您好,可以加个联系方式吗,有个PGA308 的问题要请教一下