This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

音频变压器的设计问题

现在想做一个放大模拟音频信号的音频放大器
我现在知道我的D类功放是双声道,功率为2*40W
而且想做成定压式功放,那么经过变压器输出的电压值要为120V有效值
所以,想知道如何设计音频变压器的细节
因为
【1】变压器工作频率很宽200Hz-12kHz,频带这么宽,变压器怎么满足?
【2】匝比的计算以及匝数的计算
【3】怎么满足2*40W的容量,这要设计变压器的那哪个参数来实现?
初次之外,也可以说的更加详细
  • 变压器工作频率很宽200Hz-12kHz,频带这么宽,变压器怎么满足?确实不容易满足, 只能尽量满足范围, 可以用铁氧体类的磁芯.
    匝比的计算以及匝数的计算, 还是和普通变压器一样的计算.
  • 变压器设计核心方程只有一个:E=4.44FNQm 按此计算吧。F越低;低音越好。高保真产品工作频率建议定在60~15kHz,公共广播;建议定义在60~3kHz。按低频设计;按高频控制变压器漏感。
    关于铁芯,建议用0.15~0.25mm冷轧硅钢片或超微晶铁基磁材。市面上有成品磁芯和变压器销售,有些可支持定制。