This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA828仪表运放在单电源5V供电时,第一级无法放大

Other Parts Discussed in Thread: INA828

INA828仪表运放在单电源5V供电时,第一级无法放大.DOCX设计使用INA828放大温度检测的电压信号,电路基本架构如下:

使用单5V电源供电,CN1是一个PT1000的RTD电阻,INA828放大前端惠斯通电桥的电压差,放大倍数设置的是32倍左右。最大压差设计在100℃时,RTD电阻:1.38KΩ,两端压差:0.1258V,放大之后的输出电压设计是:4.05V左右。

问题是:实际电路发现运放基本无输出,无论前端压差多少,输出都是0.007mV;

INA828的规格书中有个参考电路:

所做过的调试措施有:

1、  调整前端电桥的分压阻值;

2、  调整前端压差;

3、  按照参考电路加上从芯片输出到同向端的100K电阻;

以上措施芯片输出都是0.007V

4、怀疑芯片一脚不正确,反向焊接,输出不正确;

另外,想确认一下芯片的一管脚在哪?

芯片实物没有点,是有一条横线,一般情况下横线在上,左上角第一个PIN是芯片一脚吧,这个问题就是想确认一下。