This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA仿真运放扩压电路,带载时幅值上不去

Other Parts Discussed in Thread: OPA552, OPA2544, OPA2541, OPA544, OPA541

最近看到一个关于扩大运放输出范围的电路,但是实际用TINA仿真,会出现功率减小的问题。不知道如何改进,如下图,计算公式也如图中所示。

然后我按照这个图形在TINA中搭了一个电路,输入为4V,放大倍数为5倍。空载放大倍数正常输出20V,但是带载100mA就出现5V电压跌落。选用的OPA522最大可输出400mA左右。

然后我把上管断开,直接接入30V,这个时候就完全正常了。

所以应该是上面三极管的问题,但是这个管子最大输出电流可以到达1A,不知为什么会限制了这个扩压电路的输出功率,请问这个电路由什么改进的地方吗?