请教下,ti的工程师,我设计了一块线路板,上面用到了ti的信号调理芯片PGA309,用AD芯片采样PGA309的输出电压,然后给单片机处理,芯片调试好了,效果也还可以,但是遇到一个棘手的问题,就是应用过程中给板子上电,会经常出现PGA309输出电压会无缘无故的消失,变为0,还请各位给看看,是何原因???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教下,ti的工程师,我设计了一块线路板,上面用到了ti的信号调理芯片PGA309,用AD芯片采样PGA309的输出电压,然后给单片机处理,芯片调试好了,效果也还可以,但是遇到一个棘手的问题,就是应用过程中给板子上电,会经常出现PGA309输出电压会无缘无故的消失,变为0,还请各位给看看,是何原因???
你是不是将PRG引脚和VOUT接在一起了?如果是的话,输出先Enable一段时间然后再disable这是正常现象。
你好,谢谢你的回答,我用的是单独的4线模式,单独的两个接口,一个one wire 和 prg,不知道是啥原因??