This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1301隔离模拟信号

Other Parts Discussed in Thread: AMC1301

我想用AMC1301隔离模拟输入信号;

信号属性:正弦波,频率-10kHz,幅值:5V.单端信号,不是差分信号。

AMC手册里面写的输入范围±250mV,固定增益是8.2,但是手册里面的表格6.1显示VINP的范围是(GND1-6)至(VDD1+0.5)。那么我的输入信号幅值为5V可以吗?还有固定增益是8.2,如果不能输入5V信号,在AMC1301前端把信号降低至250mV一下,是不是就可以隔离放大输出?