This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

opa551运放输出电流有问题

Other Parts Discussed in Thread: OPA551, TINA-TI

使用opa551运放搭建可变恒流源,如上图所示。

其中,VG1为可调电压源,通过调节VG1的电压值,获得不同的输出电流。用Tina-TI仿真完全没有问题,结果如下图所示

在测试过程中,没有连接负载,直接将电流表串在电路中,测量恒流源输出电流,此时输出电流不正常,可输出的最大正电流只有20mA,仿真结果为41.68mA。最大可输出负电流 可达到-60mA,仿真结果为-41.68mA。将负载连接,再通过电流表测量,则与仿真结果吻合。原因是什么。

还有运放的正负输入端存在0.3V的压差。

请各位大佬指教指教