This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

光电检测电路

Other Parts Discussed in Thread: TLC2201, MSP430F5529, NE5532, LOG112, TPS62170, LM2660

 

背景:目前遇到一个项目,做光电检测的,使用的传感器是滨松的S1336-44BK(数据手册见附件),在实际使用中传感器能达到的峰值电流最大为250nA,之前做过一个板子,用的是TLC2201和NE5532做两级放大,后面用MSP430F5529自带的ADC采样,采样速率为100HZ左右并将数据通过串口传到PC,但噪声较大,之前的板子在布局方面也没做好,因此准备重新设计

 

我在ADI 官网用的在线仿真工具,系统给我推荐的电路图如上图所示,使用的是ADA4637-1做两级放大,放大后最大输出电压为2V附件是仿真报告(见附件)。

 

在TI官网,使用在线仿真工具WEBENCH时,放大电路只有一级放大,导致反馈电阻要选择8MΩ,这种设计显然不够合理。

 

目前想使用TI的方案来做这个电路,该部分准备单独做一块板子,实际上是做na级电流放大的方案,目前有如下问题:

 

  1. 请推荐TI的合适的运放芯片,并给出合理放大方案
  2. 由于运放要使用双电源供电,这块板子我准备用3.7V锂电池供电,准备使用±3.3V给运放供电,请推荐合适的降压芯片,能产生-3.3V的电压,并使电源纹波尽可能小
  3. 根据第一版的设计经验,该电路应该要加滤波电路,请推荐合适的滤波电路
  4. 该项目中,待测物会由步进电机拖拉平移,步进电机是通过MSP430F5529控制A3967运动的,因此在地线的处理上该注意些什么问题。

5.此类微弱电流信号的检测,在板子的布局上该注意什么问题。

 

谢谢!!

 

 Attachement.rar