This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求教:LMV321IDBVR 输出电流过大,有何方法可以缩减输出电流?

Other Parts Discussed in Thread: TLV271, LMV321

LMV321IDBVR 

目前我们在使用一款轨到轨的运放,用来做电流检测,原理图如下:

  BAT略高于GND(mA级别),  VCC= 3V3,  ADC_BAT直连到MCU的IO口,输出电流在90mA左右, 比之前用的器件要略高出50mA,目前想把输出电流降低,从规格书上观察是GAIN值与原器件在同一RL,RC上不同,相同条件下,只要把LMV321IDBVR 换成主器件,电流就会降下去,换回新的LMV321IDBVR 电流又会增加到80mA甚至100mA;

 

已尝试方法:

. 通过修改R18(RL-从10K改到47K)及C26(CL-100pF改到500pF)的值来变更GAIN,结果不理想;求教:LMV321IDBVR 输出电流过大,有何方法可以缩减输出电流?

 

  • 1. 如果您是做电流检测,从您的电路来看,既不是高侧方式也不是低侧方式来检测电流,如果您是做电流检测,可以考虑通过我们专用的电流感应放大器器件来做,电流感应放大器参考这个链接:www.ti.com.cn/.../products.html
    2. 而从您的电路来看GND与BAT_GND是什么关系?电路需要共地。您的输入信号是什么?
    如果您认为LMV321输出电流过大,可以选用输出电流小的运放,如TLV271:www.ti.com.cn/.../tlv271
  • 感谢回复!
    1.关于替换料,未来可能考虑采用其他专门器件,感谢提供此信息;
    2.BAT_GND为电池地,GND为PCBA的地,相对来说GND与BAT_GND有mA级的压降,可认为输入信号则为这个压差;
    我们认可LMV321的输出电流,但是有可否在不改用其他器件的同时,有效减小输出电流的方法吗?
    盼复,感谢
  • MCU的ADC端口是不是配置不对,正常的ADC采集端口应该配置为模拟输入,这种状态MCU不会灌入大电流,LMV321之所以输出很大电流是因为MCU侧的配置问题。MCU侧需要多大电流LMV321就提供多大,这个电流不由LMV321决定。

  • 感谢回复;
    ADC端口配置应该没有问题,因为我之前有用另一个元器件,输出的电流基本维持在30mA左右,而现在用LMV321,电流才突然变得这么高,假如我在PCBA上把LMV321换上原来的器件,那电流会掉下去。请知悉