This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA1620 EMIRR相关问题

Other Parts Discussed in Thread: INA1620

客户需要找一颗噪声在5nV/HZ以下,EMIRR在80dB以上的运放,找了一下,发现INA1620这一颗

结果它的参数是EMIRR IN+,没太懂意思,请问这个指标跟EMIRR指标有啥区别

http://www.ti.com.cn/cn/lit/ds/symlink/ina1620.pdf

  • 测量EMIRR的方法有很多,这里的EMIRR IN+指的是将RF信号作用在INA1620的IN+端进行测试的,datasheet中有相应的描述:
    Measuring EMIRR can be performed in many ways, but this section provides the EMIRR IN+, which specifically describes the EMIRR performance when the RF signal is applied to the noninverting input pin of the op amp. In general, only the noninverting input is tested for EMIRR for the following three reasons:
    • Op amp input pins are known to be the most sensitive to EMI, and typically rectify RF signals better than the
    supply or output pins.
    • The noninverting and inverting op amp inputs have symmetrical physical layouts and exhibit approximately
    matching EMIRR performance.
    • EMIRR is easier to measure on noninverting pins than on other pins because the noninverting input pin can
    be isolated on a PCB. This isolation allows the RF signal to be applied directly to the noninverting input
    terminal with no complex interactions from other components or connecting PCB traces.
  • 明白,感谢
    有一些器件没有这个EMIRR IN+的图表,那我怎么查询EMIRR值呢?
  • 我看了下,比较新的运放产品一般会有EMIRR和频率的曲线,之前的产品datasheet中确实没有给出。所以如果需要的话,可能需要去美国e2e咨询下。