This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于LMV344 3V电压跟随问题

Other Parts Discussed in Thread: LMV344

TI工程师:

          您好!我使用LMV344构建跟随电路作为28377参考电压源的buffer,替代了controlCARD参考设计OPA4350EA。原始图如下图。因为是产品批量后,才暴露出的问题,麻烦及时帮助定位和解决。

我自己的原理图如下

这里面有一个错误,就是把运放直接连接在22uF电容。但这个错误,并没有立即暴露出来。因为使用了2个批次的LMV344运放都工作正常。直到最近出现了异常。异常现象表现为,REF_IN(LMV244的10脚,12脚,5脚)电压不是3V,而是0.9~2.7V之间。我想请教的问题如下:

1、运放输出和电容之间串入的电阻,阻值如何计算?是短路电流影响还是运放的闭环带宽影响?我串入了10R,22R,200R都不在正常。不正常体现在REF_IN(LMV244的10脚,12脚,5脚)电压不是3V,而是0.9~2.7V之间。很多时候,开始还是正常的,后面就跌落了。这是什么原因呢?按理来说,串入200欧姆,已经是一个很大阻值了。有一块电路板换成1K的电阻,正常,更多实验还在测试中。

2、上电前REF_IN(LMV244的10脚,12脚,5脚)对地电阻大于40K。上电后,出现REF_IN对GND电阻值小于1K,我用万用表测得700欧姆,500欧姆等。而把芯片从电路板焊下来,不论芯片还是电路板都再次恢复高阻大于40K。这是什么原因?

3、在3.3V供电情况下,跟随电路,vin+最大允许输入多大电压?因为我在TI官网仿真,提示我不能超过2.5V,这个不是轨道轨的吗?我用了那么多输入3V也没有问题啊?

3、如何根据DSP的VREFHI,选择合适的运放作为BUFFER?当初是参考了其它品牌的开发套件选择这个运放,因为价格便宜。LMV344不能如此应用吗?可以推荐价格较低封装是TSSOP (14)的运放吗?28377的VREFHI要求如下图。

4、选定运放后,如何确定,串入的电阻值?