This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

单电源精密整流电路

Other Parts Discussed in Thread: TLV2333, OPA2626

使用TI推荐的单电源精密整流电路,我的原理图如下

但是我使用TLV2333如下

在负向翻转到正向的时候出现一个台阶,于是我将VSS由地改成了-0.2V,图形如下:

可以发现,感觉就像没有响应过来,而且随着频率增高,这个时间会有所缩短,但阶跃幅值会增高。1000Hz有88us。

于是我将TLV2333换成了手头上有的高速运放OPA2626,波形有所改善,如下图所示:

但是当我把电压升高时,会出现如下情况:

当输入信号太高到1.2V以上时,正向反而不行了,看输入共模信号到1.2V就不行了。我把电源改成了5V供电也不行。

TLV2333的就更差了,如下图:

我看资料上写TLV2333的共模能到VCC-0.3,OPA2626能到VCC-1.3,而我的VCC已经太高到+5V了,不知道这里的问题出在哪里?请各路大神指教!!!