This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电荷放大器选型以及宽幅值范围运放方案选型

Other Parts Discussed in Thread: LF356, INA326

目前有个案子,

1、在压电片后面接电荷放大器,请问下有没有合适的运放选型可以提供一下,要求增益范围10k-900khz,可以更宽。

2、同时,由于压电片的输出幅值在10mv-1v之间,要将该信号放大至合适范围给adc,不知道有没有合适的方案可以做,目前想到的有用比较器做第二级增益切换,防止信号饱和。

有没有哪位大侠帮忙提供一下电荷放大器的选型,以及在选择电荷放大器时主要考虑哪些参数呢。

  • 电荷放大器的反馈电阻非常大,通常在150M欧姆以上,如果要制作频带响应非常好的电荷放大器,则反馈电阻必须在1G欧姆以上,甚至可能到200G欧姆。而低噪声的OP37放大器的偏流在15nA左右,足以在1G欧姆(我通常用1G欧姆的反馈电阻)的反馈电阻上产生15V的输出偏压!!!所以一般要使用JFET输入型的运放,输入偏流在30pA的LF356适合做一般性能的电荷放大器,1G的反馈电阻导致450mV的输出偏压是可以通过电容隔直耦合消除的。所以我见到过很多国产的电荷放大器里面使用这款芯片。

     

  • 10mV~1V 之间宽电压范围的运放可以考虑仪表放大INA326这款。INA326的Voffset最大为100uV。输入10mV~1V为线性输入,仿真如下: