This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

高功率高带宽毛刺放大器方案

Other Parts Discussed in Thread: OPA541, THS3092

请求专家们帮忙出一个方案,核心选择哪一款放大器可以达到或者接近以下的设计指标 ,感谢

用途:高功率毛刺放大器可为任何连续消耗高达10安培和15安培峰值电流的设备提供电源。它能够传递用户设定的毛刺(该毛刺在电源上)。

指标:

信号输入

  • 电压范围+/- 2V
  • 输入阻抗50Ω

信号输出

  • 电压范围+/- 4V
  • 电流范围连续+/- 10 A和峰值+/- 15 A
  • 输出阻抗<25mΩ

获得

  • 2x(信号输出/信号输入)
  • 频率范围(DC)– 50 MHz时为3dB,100 MHz时为–6 dB,200 MHz时为–9 dB