This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

寻求一个高输入阻抗,低输入电容(共模,差模)的运放

Other Parts Discussed in Thread: OPA357, OPA338, OPA355

前级电路是一个震荡电路。为典型的电容三点式震荡电路,由于其带载能力超级弱,想寻求一款运放做跟随,震荡器输出的信号是振幅为2.1V带有2.6V的直流偏置的正弦波,频率为8MHz,现在想将这个信号用运放跟随出来,,对运放的要求是高输入阻抗,低输入电容(共模,差模),宽范围的输入,轨道轨输出,求推荐一款运放能满足该需求

  • 您好,根据您的描述,建议选择CMOS 工艺的运放,CMOS工艺运放的特点就是输入阻抗高,输入偏置电流和输入失调电压都比较小,rail to rail output 等特点,比如OPA3xx系列,OPA355, OPA338, OPA357等。
  • OPA355这个运放目前再用,很不错,但是针对这个应用场景不太合适,手册里面共模输入范围Vcm的最大值是VCC-1.5,这个条件不行,因为我的输入信号最大值为4.7V,这样会造成输出的峰值出现削波失真
    OPA338这个运放带宽和压摆率不符合要求
    OPA357这个可以尝试以下
  • 好的,我以为您的信号振幅是2.1V指的是Vpp,这样的话,2.6V偏置,信号是1.65V~3.65V的信号,OPA355的话,5.5V供电,最大输入共模电压为4V。所以误解了您的意思。 OPA357是轨至轨输入输出,所以可以满足要求。
    如果还有什么问题,请再联系。