This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH7324比较器输出一直是高电平

Other Parts Discussed in Thread: DAC7311, LMH7324, MUX36D04, TLV3604, LMH7322

电路原理图如上,LMH7324的负输入电压由DAC7311来提供,现在这个板子调节VDAC电压(0.5,1V,1.25V),输入电压输入一个正弦波,1KHz或者1MHz都测试过,正弦波分别设置为对应VDAC电压的offset,1Vpp的幅度,但是比较器LMH7324的输出2脚和3脚都是高电平,没有任何电平变化。后面我把PNA5V改成了GND,两个输出还是高电平。

请问一下,是哪里有问题?VCCO不能接+5V吗?

  • 您好,
    LMH7324可用于不同逻辑系列之间的接口,例如,可以从负电压电平的逻辑,如ECL,转换为正电压电平的逻辑,如RSPECL和LVDS,反之亦然。数据手册也提供了Figure 17、18、19、20典型电路
    您输入的电平范围是什么
  • 输入的电平范围是-5V~+5V,我理解应该是Figure 19. ANALOG TO LVDS这个电路结构,只是我把输出的电源也接到了5V,不是2.5V。然后负端的电压也不是0V,而是DAC7311给出的一个比较阈值电压。
    不清楚问题点是不是在输出电源VCCO这里?还有输入电压范围可以到±5V吗?DAP这个PAD要接GND还是接VEE?
  • 输入电压范围为VEE ~ VCCI−2V,输入信号范围是-5V ~3V
    DAP(Die-Attach-Paddle)起到散热片的作用,这意味着可以使用该焊盘下方的通孔将热量传输到任何合适的铜板上。DAP与所有其他电气连接隔离,因此可以将该焊盘连接到零件允许电压范围内的任何电压。使用DAP连接,通常的做法是将这样的焊盘连接到最低的电源电压。然而,在高频设计中,将该焊盘连接到另一个电源(例如接地层)是有用的,而VEE电压为-5V
  • 去掉LMH7324的输出串联电阻R112和R115,J11通过信号发生器33500B输入正弦波,正弦波的频率为1KHz, 幅度为500mVpp,Offset为1V。控制DAC7311输出VDAC=1.02V,用示波器测试输入信号以及LMH7324的输出3脚QA波形,如下:

    通道2为比较器LMH7324的输出QA信号。

        输出信号后的电路为:

    把MUX36D04的A0和A1脚配置为00,MUX输出选择S1A和S1B。重新接上电阻R112和R115,再次测试LMH7324的输出,R112和R115两端电压都变为了5.09V,MUX36D04的输出DA和DB也都是5.09V。这里的电压PP5V为5.10V。

    MUX36D04的输出TRIG_SIG_5V_P 和TRIG_SIG_5V_N通过一个电平转换芯片接FPGA的IO。


    这里MUX36D04会影响LMH7324的输出,问题在哪里?怎么修改?

  • 比较器LMH7324的输出QA信号是低电平4.06V高电平4.46V吗
    您有尝试断开R118和R120测试MUX36D04的输出吗,看是什么电压
  • 比较器LMH7324的输出QA信号是低电平4.06V,高电平4.46V。

    断开R118和R120测试MUX36D04的输出,有波形,DA的波形如下:

    高、低电平不变。

    MUX36D04后的电路如下:

    通过电平转换芯片TXS0104后接FPGA的IO管脚。

  • TXS0104的输入高电平和低电平最大最小如下截图,5V供电的话,若输入大于4.6V则被认为是高电平,若输入小于0.15V则被认为是低电平。其他值则不能确定是什么电平

    MUX36D04的输出电压或者说TXS0104的输入电压,不满足其电平范围

    可以看TXS0104数据手册8.2 Functional Block Diagram,TXS0104的输入信号被内部上拉电阻10K拉至VCCB了

  • 那有没有比较器支持DC~500MHz、-5V~+5V输入,比较器输出的低电平是0,高电平是电源电压的?单端输出也可以。

  • 500MHz信号,信号周期为2ns,TI的高速比较器中,只有LMH7324、LMH7322、TLV3604还有可能满足要求,但是TLV3604供电范围不满足要求,LMH7324、LMH7322即是您目前使用的产品,一个是双通道的一个是4通道的,因此TI 没有满足您要求的比较器