This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电流反馈型CFB运放之【18】

我们分析电流反馈型运放还是从它的1/2电路开始,如前面提到的原理图,(见下图)

从电路上可以看出这个电路的Q1构成的第一级放大电路的增益为R1/Re。而由Q2组成的第二级电路的直流增益(注意是直流信号)为R2/R3。由Q组成的最后一级放大电路也即为输入级电路是一个射极跟随器。其直流电压放大倍数为1。这样就可以得到整个电路的真流增益为

  

上面的公式可以视为直流开环增益。以前的博文中,一再提到运放都会有一个主极点,CFB运放也不例外。这个主极是由Ct和R1共同设定的。如下式:

注意,这个公式忽略一了些三极管的参数如Q1的射极动态电阻Re1。另外Ct是通过米勒效应乘上R3/R2。并成为Q1共射极电路的负载的。由于RE是由反馈网络决定的。我们定义互阻抗的为:

则此时放大电路的直流增益和主极点频率如下所示:

 那这个互阻抗和电容是多少呢?在有些数据手册中会给出来。如下便是电流反馈型运放OPA603的datasheet中给出的RT和CT的值: 一般CT比较小。

此时CFB运放的开环增益就可以写成如下的公式了

仔细端详这个公式就会发现,CFB运放的开环增益不仅由内部的RT和CT决定。而且由反馈网络所决定。这是从原理上,与电压反馈型运放的不同点。