TAS5711/TAS5707 datasheet上面提到的功耗,在RESET状态下,IDD功耗为24mA,但是没有提到在PDN有效时,powerdown时功耗,请问这个时候是多少?如果RESET与PDN都active时,功耗又是多少?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TAS57xx在正常工作时候,将PDN拉低,此时这时候的功耗是吗?对的,我想要的就是这个。因为实际应用中,把PDN拉低可以把声音停下来,释放后声音又有了。比Reset状态更常用。
另外的我在TAS5706的datasheet中看到了另外一个关于功耗的问题。TAS5706中,写到PDN拉低时,Idd为8mA。请问TAS5711是同样的情况么?还有TAS5706中,还有一个Icc 静态电流在power down与Reset状态的功耗,均为58uA,这个又是怎么理解。quiescent supply current与Input supply current在PDN/Reset还有区别?
谢谢