This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

3254 I2S接口问题

我们使用TI的3254,和3204,TAS5730M,他们的I2S都有MCLK信号,不知道I2S中的MCLK起到什么作用。如果我们的模块上没有MCLK输出他们还能连接吗,可不可以不用连接MCLK,或者通过一个单独的外部有源晶振给3254,3204,5730提供MCLK,而这个外部晶振与我们模块上的时钟没有任何关系。

ps:这些芯片工作在从模式,理论上master只需要提供LR CLK,BIT CLK两个时钟就可以正常通信了,为什么还要MCLK呢,是不是这个MCLK另有作用,如给芯片内部的其他数字电路提供时钟,如3254内部的DSP,如果这样理解,是不是就可以像我上面提到的直接使用一个独立的,与master没有任何连接的外部时钟提供给这些芯片作为MCLK(与LR CLK,BIT CLK没有同步关系,甚至频率不是倍数关系)?